Silicon Labs Simplifies Energy Profiling for Power-Sensitive IoT Applications
New Release of Simplicity Studio™ Development Platform Features a New Real-Time Energy Profiler Tool and Other Enhancements
AUSTIN, Texas--(BUSINESS WIRE)-- Silicon Labs (NASDAQ: SLAB), a leading provider of microcontroller, wireless connectivity, analog and sensor solutions for the Internet of Things (IoT), today announced a new release of the Simplicity Studio™ development platform designed to make IoT system design easier, faster and more productive. The industry's first IoT development platform enabling concurrent microcontroller (MCU) and wireless design, Simplicity Studio now features an enhanced real-time Energy Profiler tool, faster execution speed and an easier installation process.
Battery-powered IoT applications, such as wearables, personal medical devices, wireless sensor nodes, and gas and water meters, require exceptional energy efficiency for extended battery life. Extrapolating system-level energy consumption and battery life expectations from MCU and wireless IC data sheets is both challenging and time-consuming. Silicon Labs' new Energy Profiler helps developers optimize their IoT designs for ultra-low energy and long battery life by providing a more intuitive user interface, improved usability, and greater energy profiling accuracy and reliability.
The Energy Profiler tool offers a new Energy Score feature that is unique to the embedded industry, enabling developers to benchmark the energy efficiency of their IoT system designs. The Energy Score helps developers determine which design iteration provides the highest score directly correlated to battery life. A higher score (on a 0 to 10 scale) indicates lower energy consumption and longer battery life. The Energy Profiler also allows developers to save sessions, enabling them to compare relevant data from their saved sessions to gain a better understanding of how design modifications impact overall energy efficiency.
The Energy Profiler features an enhanced energy graphing capability that has the familiar look and feel of an oscilloscope. The developer can now zoom in on the X (time) and Y (power) axes of the energy graph to analyze the details of energy consumption with greater precision. In addition, the profiler provides a direct correlation between the energy graph, function analyzer and application code. This three-way correlation capability enhances the developer's ability to optimize designs for ultra-low energy consumption.
Silicon Labs improved the efficiency of downloading and using Simplicity Studio to help developers get their projects up and running faster and more efficiently. The size of the Simplicity Studio installation package has been reduced by a factor of ten, enabling developers to visit Silicon Labs' website, download Simplicity Studio and run a demo in less than ten minutes. In addition, the most frequent tasks in Simplicity Studio, such as software examples and demos, now run up to three times faster than they did in the previous version.
"Today's developers not only require ‘faster, smaller, cheaper' silicon from their semiconductor suppliers, they also expect continuous enhancements in development ecosystems to help them reduce energy consumption and speed time to market," said Daniel Cooley, vice president and general manager of MCU and wireless products at Silicon Labs. "We are closely attuned to the needs of our growing developer community and continue to enhance Simplicity Studio to make it the most productive, efficient and full-featured development platform in the embedded industry."
About Simplicity Studio
The Simplicity Studio platform simplifies the process of developing IoT applications by providing MCU and wireless developers with one-click access to everything they need to complete their projects, from initial concept to final product, in a unified software environment. Simplicity Studio includes an Eclipse-based integrated development environment (IDE), graphical configuration tools, energy profiling and battery estimation tools, network analysis tools, demos, software examples, documentation, technical support and community forums. All of these integrated features combine to make embedded development simple and productive for IoT developers. Simplicity Studio provides built-in intelligence to automatically detect the connected 8-bit or 32-bit MCU or wireless IC, graphically configure the device, and show supported configuration options to help developers get their projects up and running in minutes.
Silicon Labs will regularly update the Simplicity Studio platform with new and enhanced features and support for new MCU and wireless products. Before releasing new platform versions, the company plans to beta-test key features with selected customers in Silicon Labs' embedded developer community.
The latest release of Simplicity Studio including the enhanced Energy Profiler is available to developers at no charge and can be downloaded by visiting www.silabs.com/simplicity-studio.
Silicon Labs
Silicon Labs (NASDAQ: SLAB) is a leading provider of silicon, software and system solutions for the Internet of Things, Internet infrastructure, industrial automation, consumer and automotive markets. We solve the electronics industry's toughest problems, providing customers with significant advantages in performance, energy savings, connectivity and design simplicity. Backed by our world-class engineering teams with unsurpassed software and mixed-signal design expertise, Silicon Labs empowers developers with the tools and technologies they need to advance quickly and easily from initial idea to final product. www.silabs.com
Cautionary Language
This press release may contain forward-looking statements based on Silicon Labs' current expectations. These forward-looking statements involve risks and uncertainties. A number of important factors could cause actual results to differ materially from those in the forward-looking statements. For a discussion of factors that could impact Silicon Labs' financial results and cause actual results to differ materially from those in the forward-looking statements, please refer to Silicon Labs' filings with the SEC. Silicon Labs disclaims any intention or obligation to update or revise any forward-looking statements, whether as a result of new information, future events or otherwise.
Note to editors: Simplicity Studio, Silicon Labs, Silicon Laboratories, the "S" symbol, the Silicon Laboratories logo and the Silicon Labs logo are trademarks of Silicon Laboratories Inc. All other product names noted herein may be trademarks of their respective holders.
Follow Silicon Labs at http://news.silabs.com/, at http://blog.silabs.com/, on Twitter at http://twitter.com/siliconlabs and on Facebook at http://www.facebook.com/siliconlabs.
Explore Silicon Labs' diverse product portfolio at www.silabs.com/parametric-search.
View source version on businesswire.com: http://www.businesswire.com/news/home/20150720005070/en/
Silicon Labs
Dale Weisman, +1-512-532-5871
dale.weisman@silabs.com
Source: Silicon Labs
News Provided by Acquire Media