Silicon Labs Redefines Smart Home Connectivity with New Concurrent Multiprotocol SoC
MG26 SoCs are now generally available, providing developers with the highest performance and AI/ML capabilities
"With MG26, we're not just setting a new standard in multiprotocol wireless performance for battery-based, low-power smart home applications—we're redefining what's possible for the future of IoT connectivity with Matter," said
Further enhancing security through its Custom Part Manufacturing Service (CPMS),
MG26 SoC Powers Advanced IoT Applications and Matter
The MG26 SoC significantly advances Matter adoption with its concurrent multiprotocol capabilities, enabling integration of various Smart Home and Building devices like LED lighting, switches, sensors, and locks into both Matter and Zigbee networks simultaneously. This allows users to create automations and routines that incorporate more devices across different ecosystem.
In addition, the MG26's AI/ML capabilities using its embedded accelerator also enhance its performance in critical tasks like predictive maintenance, anomaly detection, keyword detection, vision, and more and more applications that span across the IoT. To help developers build devices capable of running advanced IoT applications, the MG26 family offers:
- Higher compute in a multicore format with an ARM® Cortex®-M33 CPU and dedicated cores for the radio and security subsystems, freeing up the main core for customer applications.
- Doubled Flash, RAM, and GPIO capacity compared to the MG24 device family, allowing IoT device builders to develop advanced edge applications that leverage larger, more accurate machine learning models for improved performance. It also allows for the processing of larger machine learning workloads like higher resolution vision.
- Embedded AI/ML hardware acceleration, enabling up to 8x faster processing of machine learning algorithms using as little as 1/6th the power compared to running on the CPU.
Silicon Labs' new AI/ML Developer Journey provides an easy on-ramp for developers to start building new models to take advantage of this processing power. - Best-in-class security with Silicon Labs Secure Vault™ and ARM TrustZone, compliant with all Matter security requirements.
- Using Silicon Labs Custom Part Manufacturing Service, MG26 devices can also be programmed with customer Matter device attestation certificate (DAC), security keys and other features in the fabrication process on demand, further hardening them against vulnerabilities.
- Secure OTA firmware updates in conjunction with Secure Boot prevent the installation of malicious software and allow for vulnerability patching.
- Concurrent Multiprotocol, enabling the ability to run both Zigbee and Matter over Thread at the same time, simplifying SKU management for the product manufacturer and ease of use for the end user.
- Industry-leading RF performance to energy-efficiency ratio, with transmission power of up to +19.5 dBm and world-leading receiver sensitivity with ultra-low TX, RX, and sleep currents enable long-life battery-powered IoT devices with superior wireless performance.
Setting the Industry Standard for Developing with Matter
Consumers want Matter devices that are secure, interoperable, and easy to use. Austrian smart lock manufacturer Nuki, which will enter the U.S. market in 2025, chose
"
Silicon Labs Leads the Way in Matter Expansion
Since its early announcement in 2024, MG26 has been recognized globally for its impressive capabilities, winning industry awards such as the Embedded Computing Design's Best in Show Award,
The Matter ecosystem is anticipated to experience significant growth, driven by new device types, enhanced security, and industry collaboration. As the leading semiconductor code contributor to Matter,
Learn more about how to develop cutting-edge Matter- and AI/ML-enable devices using
- The
Silicon Labs Matter Developer Journey - The
Silicon Labs AI/ML Developer Journey - Register for the
March 18 Tech Talk introducing the MG26 - Silicon Labs Wi-Fi SoCs with Matter support: SiWG917
To purchase or get more information on
About
View original content to download multimedia:https://www.prnewswire.com/news-releases/silicon-labs-redefines-smart-home-connectivity-with-new-concurrent-multiprotocol-soc-302385539.html
SOURCE
pr@silabs.com