Silicon Labs Introduces the Si535x Any-Rate 1-200 MHz CMOS Clock Generator

October 5, 2009

AUSTIN, Texas, Oct 05, 2009 (BUSINESS WIRE) -- Silicon Laboratories Inc. (NASDAQ:SLAB), a leader in high-performance, analog-intensive, mixed-signal ICs, today introduced the expansion of its Any-Rate Clock Generator family with the Si5355/56. The Si535x devices are made to order, 8-output CMOS clock generators capable of synthesizing four unique, non-integer related frequencies from 1-200 MHz. The Si535x clock generators provide guaranteed 0 ppm frequency synthesis error for any combination of frequencies, enabling the replacement of multiple clock ICs and crystal oscillators with a single device. Through a flexible web configuration utility called ClockBuilder(TM), factory-customized pin-controlled Si5355 devices are available in less than two weeks, enabling faster time to market while reducing the bill of materials in cost-sensitive networking, data communication, telecom access, computing and general purpose applications.

Modern hardware designs require a diverse combination of non-integer related reference frequencies for processors, memory, and peripheral interfaces (e.g., Ethernet, PCI Express, USB, wireless LAN, IEEE1394, etc.). Traditionally, custom clocks have not been available for the broad market due to the need to generate custom IC mask sets. Alternative approaches like 3 PLL and 4 PLL I2C programmable clock generators cannot guarantee 0 ppm frequency synthesis error for all combinations of output frequencies. In addition, the jitter performance of multi-PLL solutions varies significantly with device frequency configuration, increasing the risk that designs violate system-level jitter requirements. As a result, hardware designers often rely on crystal oscillators (XO) for clock generation in many applications to reduce risk.

The Si5355 leverages a single PLL architecture and Silicon Labs' proven MultiSynth fractional divider technology to provide greater frequency flexibility and lower jitter than 3 PLL or 4 PLL clock generators. Since the Si5355 can synthesize all frequencies with 0 ppm error, it can replace multiple clock ICs and crystal oscillators with a single IC. The Si5355 has consistently low jitter (50 ps pk-pk period jitter) regardless of frequency configuration, providing significant margin to system-level jitter requirements.

To further simplify design, the Si5355 can generate any combination of output frequencies from a standard, low cost 25 or 27 MHz crystal. If the device frequency plan changes, the same crystal can be reused, eliminating the higher cost associated with custom frequency crystals required by some traditional solutions. Alternatively, the Si5355 supports a 5-200 MHz reference clock input, enabling the device to be used in synchronous applications. Given the Si5355's frequency flexibility and jitter performance, BOM cost and complexity can be significantly reduced.

The Si5355 is the industry's first clock generator that can be completely customized and ordered directly online, simplifying product selection, device configuration and procurement. Silicon Labs' ClockBuilder(TM) web-based utility provides turnkey, application-specific clocks, eliminating the need for field programming hardware and software. Further, since the Si5355 does not require metal mask changes to customize clock frequencies like traditional clocks ICs, Silicon Labs can reduce the lead time associated with custom clocks from six weeks to less than two weeks.

"Silicon Labs' approach enables customers to use the simple ClockBuilder web utility to create custom clocks, revolutionizing the timing IC industry by enabling a broader range of customers to use clocks custom-tailored for their applications," said Dave Bresemann, vice president of Silicon Laboratories. "Frequency flexibility, programmability and mixed-signal innovation gives customers new options for clock generation that will prevent their timing subsystem from creating delays in their product development cycles."

The Si535x family includes the Si5356, an I2C-programmable Any-Rate 1-200 MHz spread spectrum clock generator. Spread spectrum is available on any clock output with any frequency and any spread amount, providing a level of design flexibility not available from traditional solutions restricted to providing spread spectrum on only one or two frequencies. If system-level electro-magnetic interference (EMI) testing confirms that spread spectrum is required by an application, spread spectrum can simply be enabled by pin selection without the need for component or firmware changes, further simplifying qualification testing and shortening the overall development cycle.

Pricing and Availability

The Si5355/56 products are available in a space-saving 4x4 mm 24-QFN package with samples and production quantities available now. Pricing for the Si5355 is $3.00 in 10k quantities. The Si5356 is priced at $3.60 in 10k quantities. The ClockBuilder utility is available at www.silabs.com/ClockBuilder. The Si5355-EVB and Si5356-EVB are available now and are each priced at $125 USD.

Silicon Laboratories Inc.

Silicon Laboratories is an industry leader in the innovation of high-performance, analog-intensive, mixed-signal ICs. Developed by a world-class engineering team with unsurpassed expertise in mixed-signal design, Silicon Labs' diverse portfolio of highly integrated, easy-to-use products offers customers significant advantages in performance, size and power consumption. These patented solutions serve a broad set of markets and applications including consumer, communications, computing, industrial and automotive.

Headquartered in Austin, TX, Silicon Labs is a global enterprise with operations, sales and design activities worldwide. The company is committed to contributing to our customers' success by recruiting the highest quality talent to create industry-changing innovations. For more information about Silicon Labs, please visit www.silabs.com.

Cautionary Language

This press release may contain forward-looking statements based on Silicon Laboratories' current expectations. These forward-looking statements involve risks and uncertainties. A number of important factors could cause actual results to differ materially from those in the forward-looking statements. For a discussion of factors that could impact Silicon Laboratories' financial results and cause actual results to differ materially from those in the forward-looking statements, please refer to Silicon Laboratories' filings with the SEC. Silicon Laboratories disclaims any intention or obligation to update or revise any forward-looking statements, whether as a result of new information, future events or otherwise.

Note to editors: Silicon Laboratories, Silicon Labs, the "S" symbol, the Silicon Laboratories logo and the Silicon Labs logo are trademarks of Silicon Laboratories Inc. All other product names noted herein may be trademarks of their respective holders.

SOURCE: Silicon Laboratories Inc.

Silicon Laboratories Inc.
Shannon Pleasant, +1-512-464-9254
Shannon.pleasant@silabs.com

Copyright Business Wire 2009