Silicon Labs Introduces Industry's Most Flexible Dual-Mode Bluetooth Module Solution

June 8, 2015

Easy-to-Use Module, Software Stack and Scripting Language Accelerate Applications Requiring Bluetooth® Smart and Bluetooth Classic Connectivity

AUSTIN, Texas--(BUSINESS WIRE)-- Silicon Labs (NASDAQ: SLAB), a leading provider of wireless connectivity solutions for the Internet of Things (IoT), today unveiled a dual-mode Bluetooth® Smart Ready module solution that gives embedded developers unparalleled flexibility to integrate both Bluetooth Smart and Bluetooth Basic Rate/Enhanced Data Rate (BR/EDR) wireless technologies while minimizing design time, cost and complexity. The new Bluetooth Smart Ready BT121 module from Bluegiga, a Silicon Labs company, provides a pre-certified, fully integrated, high-performance solution that includes the Bluetooth radio, microcontroller (MCU) and on-board Bluetooth software stack supported by Silicon Labs' complimentary Bluetooth Smart Ready software development kit (SDK) and easy-to-use BGScript™ scripting language.

The BT121 Bluetooth Smart Ready module and software are designed to help developers accelerate time to market and reduce development costs and compliance risks by providing a versatile, plug-and-play Bluetooth solution. The BT121 module is ideal for applications requiring connectivity to legacy devices that only support Bluetooth BR/EDR, as well the latest applications using Bluetooth Smart such as connected home, health and fitness, wearables and point-of-sale terminals. There are millions of legacy smart phones, tablets and PCs still in service that do not support Bluetooth Smart technology. Additionally, some applications require the higher throughput advantages of Bluetooth Classic technology, which Bluetooth Smart is not designed to achieve.

The BT121 module provides a "best of both worlds" solution for both ultra-low-power and high-data-rate Bluetooth connectivity applications. The module can connect to legacy devices that only support Bluetooth SPP or Apple® iAP2 profiles, for example, as well as to devices that support Bluetooth Smart. The easy-to-use BT121 module integrates a high-performance Bluetooth radio with an extended range of up to 400 meters, a low-power ARM® MCU, and a fully certified Bluetooth Smart Ready protocol stack in a compact 11 mm x 14 mm surface-mount package, making this one of the smallest Bluetooth Smart Ready modules in the market.

No RF or Bluetooth protocol development expertise is necessary to implement the BT121 module in Bluetooth designs. The module can be used as a peripheral along with an external host MCU, or applications can be embedded into the built-in MCU with the Bluegiga BGScript scripting language, creating a completely standalone design with minimal external components.

"Our new BT121 solution makes it simple and easy to add Bluetooth Smart and BR/EDR connectivity to wireless designs," said Riku Mettälä, general manager of wireless module products at Silicon Labs. "Bluetooth Smart is quickly becoming the most widely adopted wireless protocol for power-sensitive personal-area networking applications. Leveraging Bluegiga's deep wireless expertise, we continue to execute on our roadmap by introducing new Bluetooth modules and software stacks, enabling our customers to respond quickly to the largest, fastest-growing low-power wireless connectivity opportunity in the IoT."

Simplifying Bluetooth Development

Available for download at no charge from Bluegiga (www.bluegiga.com), the Bluetooth Smart Ready SDK is a set of software tools for simplifying the development of Bluetooth Smart Ready applications. Developers can access dozens of example Bluetooth Smart application profiles, which can be used as templates, enabling them to accelerate development time. Silicon Labs continues to expand its library of Bluetooth profiles as part of its roadmap to support new and emerging wireless applications and use cases.

The Bluetooth Smart Ready stack and SDK are fully compatible with Silicon Labs' recently announced Blue Gecko Bluetooth Smart modules. This compatibility makes it easy for developers to migrate their designs between Silicon Labs' Bluetooth Smart and Smart Ready modules with a consistent set of application programming interfaces (APIs) and software tools.

Pricing and Availability

Pre-production samples of the Bluetooth Smart Ready BT121 module, along with the development kit, are available now for engineering evaluation and prototyping. Volume quantities of the module are planned for Q3. For module pricing, please contact your local Silicon Labs sales representative or an authorized distributor. For additional BT121 module information and samples, please visit www.silabs.com/bluegiga.

Silicon Labs

Silicon Labs (NASDAQ: SLAB) is a leading provider of silicon, software and system solutions for the Internet of Things, Internet infrastructure, industrial automation, consumer and automotive markets. We solve the electronics industry's toughest problems, providing customers with significant advantages in performance, energy savings, connectivity and design simplicity. Backed by our world-class engineering teams with unsurpassed software and mixed-signal design expertise, Silicon Labs empowers developers with the tools and technologies they need to advance quickly and easily from initial idea to final product. www.silabs.com

Cautionary Language

This press release may contain forward-looking statements based on Silicon Labs' current expectations. These forward-looking statements involve risks and uncertainties. A number of important factors could cause actual results to differ materially from those in the forward-looking statements. For a discussion of factors that could impact Silicon Labs' financial results and cause actual results to differ materially from those in the forward-looking statements, please refer to Silicon Labs' filings with the SEC. Silicon Labs disclaims any intention or obligation to update or revise any forward-looking statements, whether as a result of new information, future events or otherwise.

Note to editors: Silicon Labs, Silicon Laboratories, the "S" symbol, the Silicon Laboratories logo and the Silicon Labs logo are trademarks of Silicon Laboratories Inc. All other product names noted herein may be trademarks of their respective holders.

Follow Silicon Labs at http://news.silabs.com/, at http://blog.silabs.com/, on Twitter at http://twitter.com/siliconlabs and on Facebook at http://www.facebook.com/siliconlabs.

Explore Silicon Labs' diverse product portfolio at www.silabs.com/parametric-search.

 

Silicon Labs
Dale Weisman, +1-512-532-5871
dale.weisman@silabs.com

Source: Silicon Labs

News Provided by Acquire Media