Silicon Labs Introduces Industry's Fastest Infrared Sensing ICs for Human Interface Applications

October 28, 2009

AUSTIN, Texas, Oct 28, 2009 (BUSINESS WIRE) -- Silicon Laboratories Inc. (NASDAQ: SLAB), a leader in high-performance, analog-intensive, mixed-signal ICs, today announced its entry into the human interface market with the introduction of the QuickSenseTM portfolio, including the Si1102 proximity sensor and the Si1120 proximity and ambient light sensor, the industry's fastest infrared sensing solutions. Optimized for power efficiency, the Si1102 and Si1120 enable touchless human interface sensing and superior detection range. Ideal for a wide variety of sensing applications, the Si1102/20 devices are well suited for products that can benefit from system power savings, tamper detection/proofing and gesture interpretation, such as portable electronics, IP phones, displays, kiosks, dispensers, interactive toys, clock radios, and other consumer and industrial products.

The QuickSense Si1102 sensor enables an electronic device to quickly gauge its proximity to the user. For example, it can detect if a handset is near a user's face and adjusts the display and lighting accordingly. The QuickSense Si1120 infrared proximity and ambient light sensor can also detect the ambient light in the external environment, allowing screen backlighting to be dimmed, for example, saving power. When paired with the F700 and F800 touch sense microcontrollers (MCUs), the QuickSense solution enables smart motion sensing, giving designers a complete array of human interface technologies for their applications and fundamentally improving the end-user experience.

Historically, designing advanced human interface features into end products has been challenging and has introduced performance and power trade offs. Silicon Labs' patented technologies and decade of infrared product design and manufacturing expertise has created a new method that eliminates the tradeoffs. Unlike competing approaches that require the infrared LED to be pulsed multiple times over a long period for accurate measurements, the Si1102/20 devices use a patented single-pulse proximity measurement technique to achieve up to a 4000x improvement in power efficiency, resulting in longer battery life, a critical feature in portable applications. With up to a 50 cm range (unaided by lenses), the Si1102/20 can easily power down displays and other functions when the user is not present. This power-saving capability is particularly appropriate for products such as appliances, security panels and IP phones.

The Si1120 device enables an innovative, patent-pending touchless proximity slider for gesturing, allowing end users to navigate without a physical touch but with simple gestures. The superior sensitivity that enables this touchless control feature has the added benefit of offering robust performance under a wide range of lighting conditions. It also enables the use of low-cost or low-profile infrared LEDs, often resulting in a significant system cost savings.

The Si1102 and Si1120 infrared sensor family is supported by the QuickSense Studio, a common development framework for all of the QuickSense devices including the F700 and F800 touch sense MCUs. The QuickSense Studio configuration wizard allows designers, using an intuitive software GUI, to select which functions they want implemented such as capacitive touch sense buttons, sliders and wheels, and then easily auto-generate the software to set up and calibrate these functions. Designers can also test their implementation and review a graphical display of the system performance.

"Silicon Labs' QuickSense human interface portfolio gives developers a robust, low-power human interface solution that's easily configurable with a straightforward development environment," said Mark Thompson, vice president and general manager of Silicon Laboratories. "No other supplier is able to match the speed and accuracy of our sensors or to combine intelligent optical sensing with touch sense MCUs, making Silicon Labs a single source for advanced, easy-to-use human interface technology."

Pricing and Availability

The QuickSense Si1102 proximity detector and Si1120 proximity and ambient light sensor are supported by reference designs and evaluation boards available at www.silabs.com/pr/QuickSense.

The Si1102 and Si1120 devices are available now in an 8-pin ODFN package and are priced at $0.90 and $1.05 (USD) respectively in 10k quantities. For more information or to request samples, please visit www.silabs.com/pr/QuickSense.

Silicon Laboratories Inc.

Silicon Laboratories is an industry leader in the innovation of high-performance, analog-intensive, mixed-signal ICs. Developed by a world-class engineering team with unsurpassed expertise in mixed-signal design, Silicon Labs' diverse portfolio of highly integrated, easy-to-use products offers customers significant advantages in performance, size and power consumption. These patented solutions serve a broad set of markets and applications including consumer, communications, computing, industrial and automotive.

Headquartered in Austin, TX, Silicon Labs is a global enterprise with operations, sales and design activities worldwide. The company is committed to contributing to our customers' success by recruiting the highest quality talent to create industry-changing innovations. For more information about Silicon Labs, please visit www.silabs.com.

Cautionary Language

This press release may contain forward-looking statements based on Silicon Laboratories' current expectations. These forward-looking statements involve risks and uncertainties. A number of important factors could cause actual results to differ materially from those in the forward-looking statements. For a discussion of factors that could impact Silicon Laboratories' financial results and cause actual results to differ materially from those in the forward-looking statements, please refer to Silicon Laboratories' filings with the SEC. Silicon Laboratories disclaims any intention or obligation to update or revise any forward-looking statements, whether as a result of new information, future events or otherwise.

Note to editors: QuickSense, Silicon Laboratories, Silicon Labs, the "S" symbol, the Silicon Laboratories logo and the Silicon Labs logo are trademarks of Silicon Laboratories Inc. All other product names noted herein may be trademarks of their respective holders.

SOURCE: Silicon Laboratories Inc.

Silicon Laboratories Inc.
Dale Weisman, +1-512-532-5871
dale.weisman@silabs.com

Copyright Business Wire 2009