Silicon Labs Demodulator Simplifies Video Front-Ends for TVs and Set-Top Boxes
Si2169 Multimedia Demodulator First to Merge All Digital Video Broadcast (DVB) Standards into Single-Chip Solution
AUSTIN, Texas--(BUSINESS WIRE)-- Silicon Laboratories Inc. (NASDAQ: SLAB), a leader in high-performance, analog-intensive, mixed-signal ICs, today introduced the broadcast video industry's most advanced, single-chip multimedia demodulator, enabling developers to simplify the design of iDTV, set-top box (STB) and Blu-ray/DVD recorder products. The new Si2169 device is the first demodulator to integrate the emerging DVB-T2 standard, advanced DVB-S2 standard, and existing DVB-T, DVB-S and DVB-C standards into a single CMOS chip supporting terrestrial, satellite and cable TV broadcast. The Si2169 is complemented by the Si2168, a pin-compatible DVB-T2/T/C demodulator designed for terrestrial and cable TV broadcast.
The Si2168/69 demodulators offer the industry's highest level of DVB-T2 terrestrial broadcast performance, outperforming other competing DVB-T2 demodulators in challenging reception conditions and fully complying with the NorDig 2.2.1 and D-Book 7 specifications. Offering superior echo performance in all DVB-T2 transmission modes, the new demodulators enable the industry's fastest DVB-T2 channel lock times under the most challenging echo conditions. In fact, Silicon Labs has implemented a special architecture to reduce DVB-T2 lock times to industry-leading values unlike competing demodulators that typically require significantly longer time to lock onto difficult channels.
When combined with Silicon Labs' market-leading silicon TV tuners, the Si2168/69 demodulators enable a complete video front-end solution from RF to baseband. The Si2168/69 architecture is also flexible enough to support other tuner options including mixer oscillator phase-locked loop (MOPLL)-based modules and standard intermediate frequency (IF) terrestrial silicon tuners.
"Leveraging our proven digital demodulation architecture, the Si2169 achieves excellent reception performance for each digital media type while reducing video front-end design complexity, power consumption and cost," said James Stansberry, vice president and general manager of Silicon Labs' broadcast products. "The combination of next-generation DVB-T2/S2 multimedia support and single-chip integration makes the Si2169 the industry's most flexible and highest-performance demodulator solution available."
The Si2168/69 devices are the smallest footprint digital TV and multimedia demodulators available, making them ideal for ultra-thin iDTV designs either directly on the main TV/STB board or inside a compact module. The Si2168/69 devices require no specific, costly components, thus simplifying the system BOM and reducing cost. The new demodulators also use only two power supplies, resulting in the industry's lowest power dissipation (450 mW typical) for the most computation-intensive DVB-T2 mode.
Pricing and Availability
Samples and production quantities of the Si2169 and Si2168 demodulators are available now in 7 mm x 7 mm 48-pin QFN packages. The Si2169 and Si2168 demodulators are priced at $9.94 and $7.92 (USD), respectively, in 10,000-unit quantities. Silicon Labs provides comprehensive evaluation platforms for video front-end designs including the DVB-T2/T/C/S/S2 Si2169 EVB containing the industry-leading Si2176 hybrid tuner and the DVB-T2/T/C Si2168 EVB containing the Si2146 digital-only tuner.
For more information about Silicon Labs' TV demodulator products and to purchase samples, please visit www.silabs.com/pr/tv-demodulator.
Silicon Laboratories Inc.
Silicon Laboratories is an industry leader in the innovation of high-performance, analog-intensive, mixed-signal ICs. Developed by a world-class engineering team with unsurpassed expertise in mixed-signal design, Silicon Labs' diverse portfolio of patented semiconductor solutions offers customers significant advantages in performance, size and power consumption. For more information about Silicon Labs, please visit www.silabs.com.
Cautionary Language
This press release may contain forward-looking statements based on Silicon Laboratories' current expectations. These forward-looking statements involve risks and uncertainties. A number of important factors could cause actual results to differ materially from those in the forward-looking statements. For a discussion of factors that could impact Silicon Laboratories' financial results and cause actual results to differ materially from those in the forward-looking statements, please refer to Silicon Laboratories' filings with the SEC. Silicon Laboratories disclaims any intention or obligation to update or revise any forward-looking statements, whether as a result of new information, future events or otherwise.
Note to editors: Silicon Laboratories, Silicon Labs, the "S" symbol, the Silicon Laboratories logo and the Silicon Labs logo are trademarks of Silicon Laboratories Inc. All other product names noted herein may be trademarks of their respective holders.
Follow Silicon Labs on Twitter at http://twitter.com/silabs and on Facebook at http://www.facebook.com/siliconlabs.
Explore Silicon Labs' diverse product portfolio at www.silabs.com/parametric-search.
Silicon Laboratories Inc.
Dale Weisman, +1-512-532-5871
dale.weisman@silabs.com
Source: Silicon Laboratories Inc.
News Provided by Acquire Media