Silicon Labs' Bluetooth® Channel Sounding Provides Sub-Meter Accuracy to Drive Secure Fine Ranging
Breakthrough Hardware and Software Boosts Bluetooth Device Ranging Accuracy and Security
Bluetooth® Channel Sounding is a new protocol stack designed to enable secure and precise distance measurement between two Bluetooth Low Energy (LE) connected devices. By offering true distance awareness, Bluetooth® Channel Sounding enhances the accuracy and security of Bluetooth device-ranging capabilities.
"In a world where location awareness is critical, Bluetooth® Channel Sounding revolutionizes proximity and location capabilities, propelling Bluetooth technology into a new era," said
Bluetooth Channel Sounding Enhances Accuracy and Security for Distance Awareness
By helping to estimate the distance between two devices, Bluetooth Received Signal Strength Indicator (RSSI) opened the door for a new wave of applications. From solutions to help locate devices like phones or tablets to digital security enhancements like geofencing, Bluetooth technology has enhanced the convenience and simplicity of everyday tasks. The challenge, however, is that Bluetooth RSSI has relied on estimations to determine location. RSSI is also susceptible to issues like multipath and obstruction which can significantly reduce accuracy. Bluetooth® Channel Sounding addresses this by improving the accuracy to sub-meter and enhancing the security of Bluetooth device ranging capabilities.
Bluetooth® Channel Sounding uses Phased-Based Ranging (PBR) to deliver precise distance measurements between two devices and a secondary ranging method called Round
With PBR and RTT, Bluetooth® Channel Sounding can be used in home and life applications like smart locks, locating consumer electronic devices, and pet trackers, as well as industrial and commercial applications like geofencing, vehicle keyless entry, and access control – all while delivering accurate, secure, and dependable Bluetooth ranging services. With advanced distance estimation techniques, Bluetooth® Channel Sounding can also be used to triangulate the position of commercial infrastructure like wireless access points or luminaires to either meet regulatory requirements or save human labor and costs.
Additionally, Bluetooth® Channel Sounding offers a more convenient and flexible ranging solution for applications that already use Bluetooth LE. In such cases, it can be implemented without the need for extra hardware and design space.
Silicon Labs New xG24 and Antenna Hardware Solutions Support Channel Sounding
Additionally, the xG24
- Single Antenna hardware has fewer antenna paths and limited multipath information, making it more suitable for basic Bluetooth® Channel Sounding applications, where lower power consumption and reliability in simpler environments are prioritized over precise distance measurement.
- Dual Antenna hardware will be available for order and use in
December 2024 . The dual antenna hardware offers higher accuracy, better spatial and enhanced multipath resolution, and is ideal for advanced applications that demand precise distance estimation such as key fobs and tags. The small form-factor of this board makes it ideal for size-constrained applications. The antenna diversity also heightens signal quality and robustness.
Qualification to version 6.0 of the Bluetooth® Core Specification for xG24 host stack and link layer are expected by the end of the year. The qualified stack will support intra-event antenna switching for optimal Non-Line-of-Sight performance and supports Channel Sounding when xG24 is operating in either NCP (Network Co-Processor) mode with an external application MCU (microcontroller unit) or SoC (System on Chip) mode with an integrated application MCU.
Get Started with Bluetooth® Channel Sounding with
- The Silicon Labs Bluetooth® Channel Sounding blog
- The Silicon Labs Bluetooth® Channel Sounding page
- Watch the Bluetooth® Channel Sounding Tech Talk
About
View original content to download multimedia:https://www.prnewswire.com/news-releases/silicon-labs-bluetooth-channel-sounding-provides-sub-meter-accuracy-to-drive-secure-fine-ranging-302236822.html
SOURCE
Sam Ponedal, sam.ponedal@silabs.com