Silicon Labs Announces Next Generation Series 3 Platform to Create a Smarter, More Efficient IoT
AI/ML Engines in Series 3 devices boost performance by more than 100x
"Our Series 3 platform is built for a more connected world that demands development flexibility and that more intelligence be pushed to the edge," said
Series 3 Platform Brings New Performance Capabilities, Efficiencies, and Diversified Supply Chain
The initial Series 1 and current-gen Series 2 platforms continue to be successful in helping to scale the IoT, connect more and more devices, and open up new applications. In large part, this is because they formed a platform with many commonalities that developers could leverage, and Series 3 follows in the same mold.
Series 3 devices will be able to answer the challenges that the continued acceleration of IoT poses: demands for more processing power at far-edge devices across all IoT applications in key areas including, but not limited to, smart cities and civil infrastructure, commercial buildings, retail and warehouses, smart factories and Industry 4.0, smart homes, personal and clinical healthcare, and the demand for increasingly portable, secure, compute-intensive applications. Series 3 advances
- More Security and Power Efficiency: Building on
Silicon Labs' industry-leading Secure Vault™ technology, the first security package to earn PSA Level 3 certification, Series 3 devices will include all the security features available on Series 2 devices with new enhancements to make them the most secure devices in the IoT marketplace. By targeting critical power points with proprietary improvements, Series 3 is designed to add years to a device's battery life. - New Levels of Compute: Series 3 will bring more than 100X processing capability, including integrated AI/ ML accelerators for edge devices, enabling consolidation of system processing into wireless SoCs. In other words, with Series 3, with the increases in programmable compute, developers can eliminate MCUs taking up space and adding cost to their systems. This will include cutting-edge digital and analog peripherals enabling higher-performance systems.
- More Scalable: Series 3 will be the only multi-radio IoT platform with a common code base for over 30 products across key wireless protocols including, but not limited to, Bluetooth LE, Wi-Fi, Wi-SUN, 15.4, multiprotocol, and proprietary protocols. This will allow developers to use one common set of tools to build applications and program countless devices. In addition, Series 3 will support an extendable, scalable memory architecture, including support for external flash.
The move to 22 nm will also open significant scalability for Series 3. The past several years have included several events and trends that have put a strain on the semiconductor supply chain across the entire industry, and the IoT hasn't been immune. In an effort to minimize geographic risk and disruptions for customers, Series 3 will be produced in multiple fabs across multiple geographies.
One of the most common pieces of developer feedback is that they don't want to be locked into vendor-specific tools, and they increasingly want to leverage open-source communities and third-party applications to enhance their development capabilities. Because of this, the biggest and most impactful change to
"We recognize that development is not a one-size-fits-all approach," said
In a move to fulfill that goal,
In addition, to be a supportive partner in the development process,
Silicon Labs Works With Developers Conference Brings the Best and Brightest to
These announcements are being made during
This document references forward-looking statements. Any such references are not a commitment, promise, or legal obligation to deliver any material, code, or functionality. The development, release, and timing of features or functionality remain at the sole discretion of
View original content to download multimedia:https://www.prnewswire.com/news-releases/silicon-labs-announces-next-generation-series-3-platform-to-create-a-smarter-more-efficient-iot-301906231.html
SOURCE
Sam Ponedal, sam.ponedal@silabs.com