Silicon Labs and Arduino Partner to Democratize Matter
Collaboration enables developers to go from new board to commissioned device in under two minutes
"Arduino's simplicity, ease of use, and powerful development environment is what makes them so appealing to their community of over 33 million users, whether they be Makers just getting started, or Pros with a wealth of development experience," said
Code samples, reference designs, documentation and more are now live in the
Arduino is an ecosystem that offers hardware products, software solutions, and cloud services accessible to all. In line with the open-source nature of the entire project, the Arduino programming language – used in the Arduino Integrated Development Environment (IDE) – has grown and evolved over the years thanks to the input of its highly engaged community and user base, who routinely contribute to the platform's ability to meet the changing needs of the embedded computing market. Its intuitive interface and extreme ease of use have made it a favorite for anyone from students taking their first steps in coding to enterprise developers. This new partnership marks a crucial step further in this direction, lowering barriers to entry to make developing a Matter device easier than ever.
"Empowering innovators has always been at the core of Arduino's mission, and our collaboration with
Indeed, Arduino's shared software resources are incredibly powerful, with a wide range of pre-compiled libraries to help developers get their new devices up and running, quickly. In internal testing,
Phase Two of Partnership Focuses on Bringing New Hardware to Market
A complete platform for Matter development needs both hardware and software, and as Phase Two of the collaboration between Arduino and
Based on the MG24 SoC, the module provides wireless connectivity using Matter, Thread, and Bluetooth® protocols. With key features like an ARM® Cortex®-M33, ten dBm output power, low current consumption, and the highest PSA Certification Level 3 security, Arduino developers can create robust, fast, and energy-efficient applications while securing end-user privacy. The large memory of up to 1536 kB of Flash, 256 kB of RAM, and 32 GPIO provides the capacity and expandability needed for Matter.
This new partnership between
- See how easy it is to program and commission a new Matter over Thread device in the Quick Look – Matter Over Thread for Arduino video on YouTube
- Read more about the partnership in Arduino's blog
About
We're a leader in secure, intelligent wireless connectivity for a more connected world. For more information visit www.silabs.com.
About Arduino
Arduino is the leading open-source hardware and software company in the world. Born to provide an easy-to-use platform for anyone making interactive projects, Arduino has reached a growing community and adapted to new needs and challenges, branching out into products for IoT, wearables, 3D printing, and embedded environments. As of today, the Arduino community includes over 33 million active users.
View original content to download multimedia:https://www.prnewswire.com/news-releases/silicon-labs-and-arduino-partner-to-democratize-matter-302054707.html
SOURCE
Sam Ponedal, 916-217-0145, sam.ponedal@silabs.com