Silicon Labs Advances Large-Scale Matter Deployments with 200-Node Matter-over-Thread Validation Network
Demonstration validates Matter readiness for commercial buildings, smart homes and next-generation IoT deployments using concurrent multiprotocol technology
Announced at the
"Matter is rapidly evolving from a smart home technology into a platform capable of supporting much larger deployments," said
Largest Public Validation Network Demonstrates Matter Scalability for Industrial and Commercial Applications
Believed to be among the largest publicly documented Matter-over-Thread performance test networks to date, the deployment was designed to evaluate how Matter performs as networks expand beyond traditional residential use cases. Unlike a controlled laboratory simulation, the network operated across
The validation effort reflects
The results come as the Matter ecosystem continues to mature and expand.
Key findings from the 200-node Matter-over-Thread validation network include:
- Successful deployment and sustained operation of a 200-node Matter-over-Thread network in a real-world office environment.
- 100% commissioning success using on-network commissioning.
- Reliable multicast and multi-hop unicast communications with mean multicast latencies as low as 87 ms and less than 1% packet loss across most payload sizes.
- Consistent operation despite active Wi-Fi, Bluetooth and Thread traffic, with no specialized topology engineering required.
- Validation that Matter-over-Thread can support commercial-scale lighting, building automation and large IoT deployments.
Silicon Labs OpenThread Border Router and Concurrent Multiprotocol Technology Provide Stable Matter Foundation
The 200-node Matter-over-Thread validation network was built using the OpenThread Border Router (OTBR) implementation, which provided the Thread network infrastructure used to commission and manage devices participating in the test. As Matter-over-Thread deployments scale, Border Routers play a critical role in securely connecting Thread devices to controllers, cloud services and broader IP networks.
The results also reinforce the value of
This capability allows manufacturers to support current customer installations while preparing for future Matter adoption, reducing development complexity, streamlining inventory management and enabling a smoother transition between ecosystems.
The complete Matter Large Network Performance report is available at: https://www.silabs.com/wireless/matter/matter-over-thread-large-network-performance-testing.
About Silicon Labs
Silicon Labs (NASDAQ: SLAB) is the leading innovator in low-power connectivity, building embedded technology that connects devices and improves lives. Merging cutting-edge technology into the world's most highly integrated SoCs, Silicon Labs provides device makers with the solutions, support, and ecosystems needed to create advanced edge connectivity applications. Headquartered in Austin, Texas, Silicon Labs has operations in over 16 countries and is the trusted partner for innovative solutions in smart home, industrial IoT, and smart cities markets. Learn more at https://www.silabs.com.
View original content to download multimedia:https://www.prnewswire.com/news-releases/silicon-labs-advances-large-scale-matter-deployments-with-200-node-matter-over-thread-validation-network-302801809.html
SOURCE Silicon Labs
Sam Ponedal, Head of PR, sam.ponedal@silabs.com