Silicon Laboratories Supports Open Standard for Wireless Control Applications
AUSTIN, Texas--(BUSINESS WIRE)--Sept. 19, 2007--Silicon Laboratories Inc. (Nasdaq:SLAB), a leader in high-performance, analog-intensive, mixed-signal ICs, today announced its support for ONE-NET, an open design standard for low-power wireless applications for residential and small business control. All of Silicon Laboratories' high-performance, mixed-signal microcontrollers (MCUs) now support this open standard for wireless control.
The ONE-NET wireless standard is specifically designed to cost effectively combine low power and a high level of security in a comprehensive design specification distributed royalty-free, accelerating the availability and use of wireless connectivity in a variety of applications. Silicon Labs' 8-bit mixed-signal MCUs integrate world-class analog with a high-speed pipelined 8051 CPU in each device and are ideally suited for low-power wireless applications. Combining high-precision analog peripherals, with a low-current consumption, high-throughput (up to 100 MIPS) 8051 CPU and up to 128 kB of on-chip Flash memory, these devices provide the optimal platform for a wide range of wireless automation, industrial, medical and residential monitoring and control applications. Low cost, easy-to-use development kits are available for all Silicon Labs MCUs to help speed system development.
"The ONE-NET community is pleased to have Silicon Labs support and welcome them to the ONE-NET open source community for wireless control," said James Martin, Director for the ONE-NET organization. "The Silicon Labs product portfolio of high-performance MCUs is excellent for ONE-NET-based designs, as it integrates cost-efficient 8-bit architecture with the high performance needed to support encoding and encryption functions that are integral to our protocol."
ONE-NET
ONE-NET is an independent, user-supported development community committed to open standards. Its ONE-NET standard for low-power wireless connectivity is optimized for residential and small business control applications; it is specifically designed to use very low power and provide very good security at a very low cost. Founding members of the ONE-NET design community; including Analog Devices, Integration Associates, Micrel Semiconductor, Renesas Technology, RF Monolithics, Semtech Corporation, and Threshold Corporation; have all committed to develop products and/or components to the ONE-NET standard. For more information about ONE-NET and the ONE-NET open design standard for low-power wireless, visit www.ONE-NET.info.
Silicon Laboratories Inc.
Silicon Laboratories is an industry leader in the innovation of high-performance, analog-intensive, mixed-signal ICs. Developed by a world-class engineering team with unsurpassed expertise in mixed-signal design, Silicon Labs' diverse portfolio of highly-integrated, easy-to-use products offers customers significant advantages in performance, size and power consumption. These patented solutions serve a broad set of markets and applications including consumer, communications, computing, industrial and automotive.
Headquartered in Austin, TX, Silicon Labs is a global enterprise with operations, sales and design activities worldwide. The company is committed to contributing to our customers' success by recruiting the highest quality talent to create industry-changing innovations. For more information about Silicon Labs, please visit www.silabs.com.
Cautionary Language
This press release may contain forward-looking statements based on Silicon Laboratories' current expectations. These forward-looking statements involve risks and uncertainties. A number of important factors could cause actual results to differ materially from those in the forward-looking statements. For a discussion of factors that could impact Silicon Laboratories' financial results and cause actual results to differ materially from those in the forward-looking statements, please refer to Silicon Laboratories' filings with the SEC. Silicon Laboratories disclaims any intention or obligation to update or revise any forward-looking statements, whether as a result of new information, future events or otherwise.
Note to editors: Silicon Laboratories, Silicon Labs, the "S" symbol, the Silicon Laboratories logo, and the Silicon Labs logo are trademarks of Silicon Laboratories Inc. All other product names noted herein may be trademarks of their respective holders.
CONTACT: Silicon Laboratories Inc., Austin
Lindsey Starnes, +1-512-532-5349
lindsey.starnes@silabs.com
SOURCE: Silicon Laboratories Inc.