Silicon Laboratories Announces Industry's Fastest, Most Integrated Four Channel Digital Isolators; Specification Compliant Si844x Isolators Speed Time-to-Market for Customers
The Si844x single-chip solution greatly simplifies circuit layout design compared to other isolation technologies implemented with multiple discrete components. Based on a patented architecture, the Si844x achieves the highest level of performance using a unique RF encoding/decoding scheme that provides a robust isolated data path and requires no special consideration or initialization. While traditional isolation methods are notoriously slow and exhibit changing operating characteristics with temperature and time, the Si844x products are as much as 1500x faster than other isolation technologies and exhibit stable operating characteristics over temperature, supply voltage and time.
"Silicon Laboratories' Si844x digital isolators stand out as exciting new products," said Chris Ambarian, senior analyst in power management with iSuppli, a leading market research firm. "iSuppli has long been saying that one of the real challenges to lowering system cost using digitalized power techniques is to find a way to cost-effectively transfer a lot of data from layer to layer within the system with negligible propagation delay. It seems that Silicon Laboratories has just provided the missing link in our vision of exactly what the next generation of power hardware architectures need."
"The Si844x is an extension of Silicon Laboratories' innovative digital power product portfolio and leverages patented technology to deliver highly integrated power solutions with unmatched performance," said Don Alfano, director of power products for Silicon Laboratories. "The digital isolator enables us to increase our offering to power supply customers by offering a single-chip, fully compliant solution that can be used in a variety of applications that require isolation, level shifting or ground-loop elimination."
The product family includes the four-channel Si8440, Si8441 and the Si8442, all of which are offered in a 16-pin wide-body small outline IC package (SOIC) that is pin-for-pin compatible with competing solutions. The Si8840 offers four forward channels while the Si8441 offers three forward channels and one reverse channel, and the Si8442 offers two forward channels and two reverse channels. The Si844x products are fully specification compliant with Underwriters Laboratories UL1577 (USA), VDE Testing and Certification Institute VDE60747-5-2 (Europe) and CSA's Component Acceptance Service CSA#5A (Canada).
Pricing and Availability
Pricing for the Si844x family begins at $2.44 in quantities of 1K. Samples are available now and production is scheduled for Q2 2006.
Silicon Laboratories Inc.
Silicon Laboratories Inc. is a leading designer of high-performance, analog-intensive, mixed-signal integrated circuits (ICs) for a broad range of applications. Silicon Laboratories' diverse portfolio of highly integrated, patented solutions is developed by a world-class engineering team with decades of cumulative expertise in cutting-edge mixed-signal design. The company has design, engineering, marketing, sales and applications offices throughout North America, Europe and Asia. For more information about Silicon Laboratories please visit www.silabs.com.
Cautionary Language
This press release may contain forward-looking statements based on Silicon Laboratories' current expectations. These forward-looking statements involve risks and uncertainties. A number of important factors could cause actual results to differ materially from those in the forward-looking statements. For a discussion of factors that could impact Silicon Laboratories' financial results and cause actual results to differ materially from those in the forward-looking statements, please refer to Silicon Laboratories' filings with the SEC. Silicon Laboratories disclaims any intention or obligation to update or revise any forward-looking statements, whether as a result of new information, future events or otherwise.
Note to editors: Silicon Laboratories and the Silicon Laboratories logo are trademarks of Silicon Laboratories Inc. All other product names noted herein may be trademarks of their respective holders. In the first paragraph above, "RMS" is a subscript term. It was changed for transmission purposes only.
CONTACT: Silicon Laboratories Inc., Austin
Tiffany Plowman, 512-464-9432
tiffany.plowman@silabs.com
SOURCE: Silicon Laboratories Inc.