Silicon Laboratories Announces Carrier Grade Dual ProSLIC for VoIP Equipment

June 4, 2007

The Si3226 Expands Industry-Leading ProSLIC® Portfolio®
In contrast to analog-based SLICs, the Si3226 is built on a highly-programmable digital SLIC architecture that provides the flexibility to support the broadest range of customer requirements. Worldwide compliance is supported using a single hardware design and bill-of-materials. The Si3226 further combines a multimode ring generator and programmable battery-tracking dc-dc controller that enable low power operation in all line states. The device leads the voice over IP (VoIP) industry in idle-channel noise performance achieving as low as 7 dBrnC using advanced noise reduction techniques.

Remote diagnostics have become increasingly important in VoIP equipment as operators seek to reduce network maintenance costs. The Si3226 is equipped with a 12-bit monitoring ADC and powerful DSP engine that enable fast and accurate reporting of subscriber line faults. Fault isolation is enhanced through the support of two independent line-sensing paths per channel: one inside of the line protection and one outside. Diagnostic tests, such as those outlined in international testing standards like GR-909, can be implemented using the Si3226 without the need for relays or dedicated test equipment.

To simplify and accelerate software development, Silicon Labs provides an extensive application programming interface (API) for the complete ProSLIC portfolio. The API provides powerful high-level commands that take full advantage of the flexibility and capabilities offered by the Si3226 while concealing the complexity of register-level programming.

"We are bringing the features, performance and reliability of traditional carrier-grade telephony to VoIP customer premise equipment," said Dave Bresemann, vice president of Silicon Laboratories. "By providing an easy-to-use API with integrated diagnostics, we're helping our customers get to market faster while reducing cost and software development overhead."

Pricing and Availability

Samples of the new Si3226 dual ProSLIC device are available now in a 64-pin TQFP, and samples of the Si3208 and Si3209 linefeed devices are available now in a 40-pin QFN. A wideband version of the device, Si3227, is also available in a pin-compatible 64-pin TQFP. Pricing for the two-channel chipsets begins at $5.79 in 10 k quantities. Silicon Laboratories' products are available in Pb-free, environmentally-friendly packages.

Silicon Laboratories Inc.

Silicon Laboratories is an industry leader in the innovation of high-performance, analog-intensive, mixed-signal ICs. Developed by a world-class engineering team with unsurpassed expertise in mixed-signal design, Silicon Labs' diverse portfolio of highly-integrated, easy-to-use products offers customers significant advantages in performance, size and power consumption. These patented solutions serve a broad set of markets and applications including consumer, communications, computing, industrial and automotive.

Headquartered in Austin, TX, Silicon Labs is a global enterprise with operations, sales and design activities worldwide. The company is committed to contributing to our customers' success by recruiting the highest quality talent to create industry-changing innovations. For more information about Silicon Labs, please visit www.silabs.com.

Cautionary Language

This press release may contain forward-looking statements based on Silicon Laboratories' current expectations. These forward-looking statements involve risks and uncertainties. A number of important factors could cause actual results to differ materially from those in the forward-looking statements. For a discussion of factors that could impact Silicon Laboratories' financial results and cause actual results to differ materially from those in the forward-looking statements, please refer to Silicon Laboratories' filings with the SEC. Silicon Laboratories disclaims any intention or obligation to update or revise any forward-looking statements, whether as a result of new information, future events or otherwise.

Note to editors: ProSLIC, Silicon Laboratories, Silicon Labs, the "S" symbol, the Silicon Laboratories logo, and the Silicon Labs logo are trademarks of Silicon Laboratories Inc. All other product names noted herein may be trademarks of their respective holders.

SOURCE: Silicon Laboratories Inc.

Silicon Laboratories Inc., Austin
Shannon Pleasant, +1-512-464-9254
Shannon.pleasant@silabs.com