New Wireless SoCs Enable Eco-Friendly Zigbee Green Power IoT Devices
AUSTIN, Texas, Feb. 19, 2020 /PRNewswire/ -- Silicon Labs (NASDAQ: SLAB) announces a new family of secure, ultra-low-power Zigbee® system-on-chip (SoC) devices designed for eco-friendly IoT products deployed in mesh networks. The EFR32MG22 (MG22) family expands Silicon Labs' Zigbee portfolio by delivering the smallest, lowest power SoCs optimized for Zigbee Green Power applications. Based on Silicon Labs' Wireless Gecko Series 2 platform, the MG22 SoCs are an ideal choice for Zigbee devices powered by coin cell batteries or energy-harvesting sources. Target applications include smart home sensors, lighting controls, and building and industrial automation.
![]()
Energy-friendly Zigbee Green Power technology can help address environmental concerns by reducing residential, commercial and industrial energy footprints, one IoT device at a time. Using the same 802.15.4 PHY and MAC of the already energy-efficient Zigbee 3.0 protocol, Zigbee Green Power further reduces power consumption by decreasing the amount of data required for wireless transmission. From its inception, Zigbee Green Power was designed to be a highly efficient protocol enabling IoT devices, whether powered by batteries or by "battery-less" energy harvesting options. Silicon Labs optimized the new MG22 SoCs to provide a best-in-class connectivity solution for these challenging, power-sensitive wireless applications.
"As the leading Zigbee provider, Silicon Labs is uniquely positioned to lead the way in Zigbee Green Power mesh networking solutions," said Matt Johnson, senior vice president and general manager of IoT products at Silicon Labs. "Our new MG22 SoC solution offers an industry-leading combination of energy efficiency, security capabilities, wireless performance, and software tools and stacks to meet the growing market demand for eco-friendly, ultra-low-power IoT products."
The MG22 SoCs incorporate a high-performance, low-power 76.8 MHz Arm® Cortex®-M33 core with TrustZone. The SoCs' combination of ultra-low transmit and receive power (8.2 mA TX at +6 dBm, 3.9 mA RX), 1.4 µA deep-sleep mode power and low-power peripherals provides exceptional energy efficiency.
Silicon Labs delivers an industry-leading suite of security features implemented in Series 2 products including the new MG22 SoCs. For more information details, visit silabs.com/security.
Pricing and Availability
The EFR32MG22 SoCs are planned to start shipping in March 2020 in a choice of 5 mm x 5 mm QFN40, 4 mm x 4 mm QFN32 and slender 0.3 mm x 4 mm x 4 mm TQFN32 packages. The EFR32MG22 SoC starter kit is planned to be available in March, with end device kit pricing starting at $99.00 (USD MSRP). Developers can download Simplicity Studio, including network analyzer and energy profiler tools, the Zigbee 3.0 stack, demos and mobile apps, at no charge. For MG22 SoC product pricing, contact your local Silicon Labs sales representative or an authorized distributor. For additional product information, visit silabs.com/mg22.
Silicon Labs
Silicon Labs (NASDAQ: SLAB) is a leading provider of silicon, software and solutions for a smarter, more connected world. Our award-winning technologies are shaping the future of the Internet of Things, Internet infrastructure, industrial automation, consumer and automotive markets. Our world-class engineering team creates products focused on performance, energy savings, connectivity and simplicity. silabs.com
Connect with Silicon Labs
Silicon Labs PR Contact: Dale Weisman +1-512-532-5871, dale.weisman@silabs.com
Follow Silicon Labs at news.silabs.com, at blog.silabs.com, on Twitter at twitter.com/siliconlabs, on LinkedIn at linkedin.com/company/siliconlabs and on Facebook at facebook.com/siliconlabs.
Cautionary Language
This press release may contain forward-looking statements based on Silicon Labs' current expectations. These forward-looking statements involve risks and uncertainties. A number of important factors could cause actual results to differ materially from those in the forward-looking statements. For a discussion of factors that could impact Silicon Labs' financial results and cause actual results to differ materially from those in the forward-looking statements, please refer to Silicon Labs' filings with the SEC. Silicon Labs disclaims any intention or obligation to update or revise any forward-looking statements, whether as a result of new information, future events or otherwise.
Note to editors: Silicon Labs, Silicon Laboratories, the "S" symbol, the Silicon Laboratories logo and the Silicon Labs logo are trademarks of Silicon Laboratories Inc. All other product names noted herein may be trademarks of their respective holders.
![]()
View original content to download multimedia:http://www.prnewswire.com/news-releases/new-wireless-socs-enable-eco-friendly-zigbee-green-power-iot-devices-301007274.html
SOURCE Silicon Labs