View all news

Silicon Labs Biosensors Add ECG Measurement for Advanced Heart Rate Monitoring in Wearables

November 29, 2017

AUSTIN, Texas, Nov. 29, 2017 /PRNewswire/ -- Silicon Labs (NASDAQ: SLAB) has introduced a family of optical biometric sensors providing advanced heart rate monitoring (HRM) along with electrocardiogram (ECG) capabilities for a wide range of wearable fitness and wellness products. The new Si117x sensor modules combine ultra-low power, high sensitivity and exceptional integration, making them ideal for smart watches and wrist-based, patch-type and other wearables requiring long battery life and enhanced HRM accuracy. To simplify development and speed time to market, Silicon Labs offers a complete, end-to-end sensing solution featuring the Si117x sensor module, HRM algorithm, Wireless Gecko SoCs for Bluetooth® connectivity, and an easy-to-use, wrist-based development kit with sample code and example projects.

Silicon Labs' new Si117x biometric sensor modules add ECG measurement for advanced heart rate monitoring in wearables.

All-day HRM is a key requirement for health and fitness wearables. By tracking HR throughout the day, end users and health-care providers can analyze physiological patterns, detect health issues before they become problems and consider lifestyle adjustments. Addressing the market need for power efficiency, the Si117x sensors consume less than 50 µA (sensor and LED combined) while performing continuous HRM. A built-in buffer and accelerometer synchronization capabilities save even more system-level power. The sensors' industry-leading power efficiency enables developers to use smaller batteries in wearable designs without significantly impacting the device's battery life during continuous monitoring.

The Si117x sensors provide enhanced HRM accuracy for a better end user experience. The sensors offer fast sampling speeds, a high signal-to-noise ratio (SNR > 100 dB), and the ability to cancel out ambient noise and erroneous data, resulting in high-quality signals that make it easier to track heart rates despite challenging physiologies, varying skin tones and the presence of tattoos. A more accurate view of the HR waveform enables biometrics beyond traditional HRM, including heart rate variability (HRV), stress analysis and pulse volume.

By combining ECG measurements with optical HR measurements, the Si117x sensors allow developers to unlock new potential biometrics for wearables. The ECG waveform is the gold standard for cardiac measurements, and the Si117x sensors bring this capability to wrist-based wearables in a cost-effective, power-efficient manner. By making measurements in the same device and at the same time, the Si117x sensors allow developers to combine biometrics with optical photoplethysmogram (PPG) measurements to derive valuable physiological parameters.

The Si117x module's high level of integration simplifies wearable design and makes it easier to synchronize multiple sensor measurements without adding significant system cost or board area. Each module supports up to four distinct LEDs (all of which can be driven simultaneously), and its four LED drivers are independently programmable (from 1.7 to 310 mA). Additional built-in features include a photodetector, 24-bit ADC with > 100 dB dynamic range, I2C and SPI digital interfaces, programmable event interrupt engine, synchronization engine, host communications processor and inputs for two external photodiodes.

"As the market for health and fitness wearables continues to grow, developers want complete biometric sensing solutions that work flawlessly without the complexities of integration," said Tom Pannell, Senior Marketing Director of IoT products at Silicon Labs. "Silicon Labs is the only supplier to provide a total HRM sensing solution in-house, from the sensor module and algorithm to the wireless SoC capable of transmitting measurements over Bluetooth LE. Our example HRM projects take care of interfacing between these components, and having a single point of contact greatly simplifies customer support and debugging."

The Si117x sensors support Silicon Labs' proprietary, motion-compensated HRM algorithm optimized for wrist-based sensing and to run on EFM32 Gecko MCUs and EFR32 Wireless Gecko SoCs supporting Bluetooth Low Energy (LE). This unparalleled integration enables system-level power and performance optimization and reduces time to market for developers seeking to add HRM capabilities to their wearable designs.

Pricing and Availability
Samples and volume quantities of the Si117x sensors are available in a 3.7 mm x 7 mm 28-pin LGA module. Silicon Labs also offers Si118x optical biometric sensors with an integrated photodiode in a clear 3 mm x 3 mm QFN package. To simplify development and performance evaluation, Silicon Labs provides a variety of wrist-based ECG and PPG development kits, a Bluetooth-enabled HRM evaluation watch, and an Android-based Triple Heart Application that captures data from multiple devices. Contact your local Silicon Labs sales representative for sensor and kit pricing. For additional information and to order sensor samples, visit www.silabs.com/hrm.

Silicon Labs
Silicon Labs (NASDAQ: SLAB) is a leading provider of silicon, software and solutions for a smarter, more connected world. Our award-winning technologies are shaping the future of the Internet of Things, Internet infrastructure, industrial automation, consumer and automotive markets. Our world-class engineering team creates products focused on performance, energy savings, connectivity and simplicity. www.silabs.com

Connect with Silicon Labs
Silicon Labs PR Contact: Dale Weisman +1-512-532-5871, dale.weisman@silabs.com 
Follow Silicon Labs at http://news.silabs.com/, at http://blog.silabs.com/, on Twitter at http://twitter.com/siliconlabs, on LinkedIn at http://www.linkedin.com/company/siliconlabs and on Facebook at http://www.facebook.com/siliconlabs.

Cautionary Language
This press release may contain forward-looking statements based on Silicon Labs' current expectations. These forward-looking statements involve risks and uncertainties. A number of important factors could cause actual results to differ materially from those in the forward-looking statements. For a discussion of factors that could impact Silicon Labs' financial results and cause actual results to differ materially from those in the forward-looking statements, please refer to Silicon Labs' filings with the SEC. Silicon Labs disclaims any intention or obligation to update or revise any forward-looking statements, whether as a result of new information, future events or otherwise.

Note to editors: Silicon Labs, Silicon Laboratories, the "S" symbol, the Silicon Laboratories logo and the Silicon Labs logo are trademarks of Silicon Laboratories Inc. All other product names noted herein may be trademarks of their respective holders.

 

View original content with multimedia:http://www.prnewswire.com/news-releases/silicon-labs-biosensors-add-ecg-measurement-for-advanced-heart-rate-monitoring-in-wearables-300562901.html

SOURCE Silicon Labs

News Provided by Acquire Media

Categories: Press Releases
View all news