Single-Chip Si534xH Clock Family Provides High-Performance,
Frequency-Flexible Timing Solution for 100G/400G Transceivers
AUSTIN, Texas--(BUSINESS WIRE)--
Silicon
Labs (NASDAQ: SLAB) has introduced a family of jitter-attenuating
clocks that simplifies 100G/400G coherent optical line card and module
design by providing a high-frequency, flexible clocking solution that
significantly reduces system-level cost and complexity. Silicon Labs'
new Si534xH coherent optical clocks replace discrete timing solutions
that rely on expensive, large-footprint voltage-controlled SAW
oscillators (VCSOs) to provide low-jitter reference timing for data
converters. Unlike VCSOs that support single, fixed frequencies, the new
Si534xH clocks operate over a wide frequency range, supporting
frequencies up to 2.7 GHz without the need to change bill-of-material
(BOM) components.
This Smart News Release features multimedia. View the full release here:
http://www.businesswire.com/news/home/20160425005076/en/

Silicon Labs Si534xH Clock Family: High-Performance Timing Solution for Coherent Optical Networks (Photo: Business Wire)
The Si5344H and Si5342H clocks combine best-in-class frequency
flexibility with unparalleled jitter performance of 50 fs RMS. The
devices simplify component sourcing, replacing multiple custom,
long-lead time VCSOs with a clock IC solution available with short,
two-week lead times. Featuring a jitter-attenuating PLL, high-frequency
output drivers, fractional frequency synthesis and digitally controlled
oscillator (DCO) technology, the Si534xH family provides all the
clocking functions required for coherent optical transceiver
applications while enabling 40 percent smaller footprint and 40 percent
lower power than competing solutions.
Get all the details about Silicon Labs' Si534xH coherent optical
clocks including data sheets, supporting documentation and development
tools at www.silabs.com/timing.
One of the largest growth drivers in the communications market is the
industry's transition from 10G to 100G in metro area networks and data
center interconnect (DCI). Coherent optics is an enabling technology for
100G and 400G applications because it allows service providers to send
more data over existing optical fiber, minimizing the cost and
complexity of network upgrades for bandwidth expansion. Current timing
solutions for coherent optics are not optimized for cost or size,
requiring a diverse mix of VCSOs, clock generators and discrete
components.
Silicon Labs' Si534xH clocks are purpose-built to address the timing
requirements of 100G/400G coherent optics. In addition to supporting the
ultra-high frequency synthesis necessary for clocking optical
transceiver data converters, the Si534xH clocks combine Silicon Labs'
proven DSPLL® jitter attenuation technology and MultiSynth low-jitter
fractional frequency synthesis technology to deliver an elegant,
easy-to-use, single-chip solution. All 100G/400G transmitter or receiver
clocks can be generated by a single device, minimizing BOM cost and
complexity by eliminating the need for numerous discrete components.
"To meet demands for increasing bandwidth, service providers require
100G/400G coherent designs that enable higher line card port density and
lower cost-per-bit than legacy solutions," said James Wilson, senior
marketing director for timing products at Silicon Labs. "Silicon Labs'
Si534xH clocks provide the high-frequency clock synthesis, jitter
attenuation and stringent phase noise required by coherent optical
applications at significantly smaller footprint and lower power than
traditional VCSO-based solutions."
Silicon Labs supports coherent clock development with ClockBuilder Pro,
an easy-to-use software tool that simplifies clock tree design, device
configuration and detailed performance evaluation. The tool can be used
in standalone mode to generate device configuration files or to directly
control a Si534xH device on an evaluation board. ClockBuilder Pro can
also be used to create factory-customized versions of Silicon Labs'
jitter attenuators and clock generators individually tailored to meet
each customer's unique timing requirements.
Si534xH Coherent Optical Clock Product Highlights
-
Ultra-high-performance jitter-attenuating PLL designed for transmitter
and receiver clocking
-
High-speed driver for data converter clocking of up to 2.7 GHz with
ultra-low phase noise
-
Typical jitter performance of 50 fs RMS (1 MHz to 40 MHz)
-
MultiSynth fractional frequency synthesis for generating any frequency
up to 712.5 MHz
-
Integrated loop filter with user-programmable PLL bandwidth for
flexible jitter attenuation
-
High-speed, digitally tunable DCO mode: 0.001 ppb resolution with 1
MHz SPI update rate
-
Module-friendly size and power consumption
-
Simple, easy-to-use ClockBuilder Pro software
Pricing and Availability
Samples of the Si5344H and Si5342H coherent optical clocks are available
now in 7 mm x 7 mm 44QFN packages, and production quantities are planned
for May. Pricing begins at $27 (USD) in 10,000-unit quantities. Standard
and custom devices are available with short lead times (two weeks for
samples and four weeks for production orders), simplifying procurement
for prototyping and production quantities. The Si5344H-EVB and
Si5342H-EVB evaluation boards, priced at $199 each (USD MSRP), are
available to simplify device evaluation and system-level timing design.
To order clock samples and evaluation boards, visit www.silabs.com/timing.
Connect with Silicon Labs
Follow Silicon Labs at http://news.silabs.com/,
at http://blog.silabs.com/,
on Twitter at http://twitter.com/siliconlabs
and on Facebook at http://www.facebook.com/siliconlabs.
Explore Silicon Labs' diverse product portfolio at www.silabs.com/parametric-search.
Silicon Labs
Silicon Labs (NASDAQ: SLAB) is a leading provider of silicon, software
and solutions for the Internet of Things, Internet infrastructure,
industrial automation, consumer and automotive markets. We solve the
electronics industry's toughest problems, providing customers with
significant advantages in performance, energy savings, connectivity and
design simplicity. Backed by our world-class engineering teams with
unsurpassed software and mixed-signal design expertise, Silicon Labs
empowers developers with the tools and technologies they need to advance
quickly and easily from initial idea to final product. www.silabs.com
Cautionary Language
This press release may contain forward-looking statements based on
Silicon Labs' current expectations. These forward-looking statements
involve risks and uncertainties. A number of important factors could
cause actual results to differ materially from those in the
forward-looking statements. For a discussion of factors that could
impact Silicon Labs' financial results and cause actual results to
differ materially from those in the forward-looking statements, please
refer to Silicon Labs' filings with the SEC. Silicon Labs disclaims any
intention or obligation to update or revise any forward-looking
statements, whether as a result of new information, future events or
otherwise.
Note to editors: Silicon Labs, Silicon Laboratories, the "S" symbol, the
Silicon Laboratories logo and the Silicon Labs logo are trademarks of
Silicon Laboratories Inc. All other product names noted herein may be
trademarks of their respective holders.

View source version on businesswire.com: http://www.businesswire.com/news/home/20160425005076/en/
Silicon Labs
Dale Weisman, +1-512-532-5871
dale.weisman@silabs.com
Source: Silicon Labs
News Provided by Acquire Media