Si1133/53 Sensors Provide Accurate Measurement of Ultraviolet
Radiation and Improved Daylight Performance and Range for Proximity
Sensing
AUSTIN, Texas--(BUSINESS WIRE)--
Silicon
Labs (NASDAQ: SLAB) has introduced next-generation optical sensors
that can be used to protect consumers from the harmful effects of
ultraviolet (UV) radiation and to develop innovative touchless user
interfaces leveraging high-performance proximity sensing and gesture
recognition. Silicon Labs' new Si1133 optical sensor provides a
cost-effective solution for adding highly accurate UV index measurement
capabilities to a wide range of sports equipment and outdoor lifestyle
products. The Si1153 ambient light sensor is optimized for operation in
bright daylight conditions and extended range, allowing it to be used
for gesture control and proximity detection applications in outdoor
environments.
Get all the details about Silicon Labs' new Si1133
UV index and Si1153
proximity/gesture detection sensors including pricing and
availability, development tools and data sheets at www.silabs.com/sensors.
Accurate UV Index Sensing
Overexposure to UV light has long been recognized as harmful, especially
for people with elevated risks of sunburn and potentially fatal
melanoma. The World Health Organization (WHO) estimates that 66,000
deaths occur annually from melanoma and other skin cancers. The Si1133
sensor enables accurate measurement of UV index levels to help gauge the
sun's intensity and prevent skin damage. The Si1133 sensor can be
incorporated easily and economically into a wide range of cost-sensitive
outdoor recreation products such as sports and fitness wearables,
backpacks, bicycle helmets, sunglasses, beach/patio furniture and sun
lotion packaging. Products equipped with the Si1133 sensor help enable
consumers to monitor their UV exposure and safely maximize their time
spent outdoors. The Si1133 UV sensor provides an output, via its I2C
serial interface, that directly corresponds to the digital UV index
defined by the World Health Organization. The Si1133 device also senses
ambient light levels, which conveniently allows for automatic brightness
adjustment of associated output displays.
Si1133 UV Index Sensor Key Features
-
Exceptional UV measurement accuracy: ±1.5 on the UV scale
-
Ambient light sensing supporting < 100 mlx resolution and operation
under dark glass
-
Highly integrated solution reducing cost and complexity with on-chip
dual 23-bit ADCs, DSP, and high-sensitivity visible light, UV and
infrared (IR) photodiodes
-
I2C serial communications with up to 3.4 Mbps data rate
-
Ultra-low power for longer battery life: 500 nA standby current
-
Small 2 mm x 2 mm QFN package
High-Performance Proximity Sensing
The Si1153 sensor offers significant performance improvements for
proximity sensing and gesture recognition in daylight conditions,
enabling a host of user interface innovations. Unlike many competing
sensors best suited to indoor environments, these new sensors can be
used outdoors in high ambient light and over an extended range of up to
2 meters. The Si1153 sensors are ideal for gesture-based operation of
automotive infotainment systems, bicycle computers and other outdoor
sports equipment, making it easier and safer for consumers to control
electronic devices without taking their eyes off the road or tasks at
hand. The sensors are also a good fit for ATMs, point-of-sale (POS)
terminals, door entry systems, and other proximity sensing applications
requiring both extended range and exceptional daylight performance.
Si1153 Proximity Sensor Key Features
-
Proximity detection adjustable from under 1 cm up to 200 cm
-
Up to 3 independent LED drivers supporting multi-axis proximity motion
detection
-
Ambient light sensing supporting < 100 mlx resolution and operation
under dark glass
-
Highly integrated solution reducing cost and complexity with on-chip
dual 23-bit ADCs, DSP, and high-sensitivity visible light and IR
photodiodes
-
I2C serial communications with up to 3.4 Mbps data rate
-
Ultra-low power for longer battery life: 500 nA standby current
-
Two package options: 2 mm x 2 mm QFN and 2.9 mm x 4.9 mm module with
LED
"Continual advances in optical sensing hold the key to product design
innovations that enhance consumer health, safety and convenience," said
Daniel Cooley, vice president of marketing for Silicon Labs' IoT
products. "Our next-generation Si1133 and Si1153 sensors provide
developers with state-of-the-art technology that makes it easy and
cost-effective to add accurate UV index measurement and high-performance
proximity sensing and gesture detection to a wide array of consumer,
automotive and commercial applications."
Silicon Labs supports optical sensing development with the 115XOPT-EXP-EVB
multi-use evaluation board, which showcases all features of the
Si1133 and Si1153 sensors and simplifies the evaluation of UV, ambient
light and proximity sensing and gesture detection.
Pricing and Availability
Samples and production quantities of the Si1133-AA00-GM UV index sensor
are available now and priced at $1.13 (USD) in 10,000-unit quantities.
Samples and production quantities of the Si1153 proximity/gesture
detection sensor are also available now in three versions: the
extended-range Si1153-AA00-GM priced at $1.84, the Si1153-AA09-GM with
enhanced daylight performance priced at $1.91, and the Si1153-AA9X-GM
module with integrated IR LED priced at $2.32 (all prices in USD and
10,000-unit quantities). The 115XOPT-EXP-EVB evaluation kit is available
now and priced at $44.43 (USD MSRP). For additional Si1133 and Si1153
product information and to order samples and evaluation boards, please
visit www.silabs.com/sensors.
Connect with Silicon Labs
Follow Silicon Labs at http://news.silabs.com/,
at http://blog.silabs.com/,
on Twitter at http://twitter.com/siliconlabs
and on Facebook at http://www.facebook.com/siliconlabs.
Explore Silicon Labs' diverse product portfolio at www.silabs.com/parametric-search.
Silicon Labs
Silicon Labs (NASDAQ: SLAB) is a leading provider of silicon, software
and solutions for the Internet of Things, Internet infrastructure,
industrial automation, consumer and automotive markets. We solve the
electronics industry's toughest problems, providing customers with
significant advantages in performance, energy savings, connectivity and
design simplicity. Backed by our world-class engineering teams with
unsurpassed software and mixed-signal design expertise, Silicon Labs
empowers developers with the tools and technologies they need to advance
quickly and easily from initial idea to final product. www.silabs.com
Cautionary Language
This press release may contain forward-looking statements based on
Silicon Labs' current expectations. These forward-looking statements
involve risks and uncertainties. A number of important factors could
cause actual results to differ materially from those in the
forward-looking statements. For a discussion of factors that could
impact Silicon Labs' financial results and cause actual results to
differ materially from those in the forward-looking statements, please
refer to Silicon Labs' filings with the SEC. Silicon Labs disclaims any
intention or obligation to update or revise any forward-looking
statements, whether as a result of new information, future events or
otherwise.
Note to editors: Silicon Labs, Silicon Laboratories, the "S" symbol, the
Silicon Laboratories logo and the Silicon Labs logo are trademarks of
Silicon Laboratories Inc. All other product names noted herein may be
trademarks of their respective holders.

View source version on businesswire.com: http://www.businesswire.com/news/home/20160118005559/en/
Silicon Labs
Dale Weisman, +1-512-532-5871
dale.weisman@silabs.com
Source: Silicon Labs
News Provided by Acquire Media