Running mbed on EFM32® Devices Will
Accelerate Deployment of Energy-Friendly Internet of Things Applications
AUSTIN, Texas--(BUSINESS WIRE)--
Silicon
Labs (NASDAQ: SLAB), a leading provider of microcontroller, sensing
and wireless connectivity solutions for the Internet
of Things (IoT), today announced a collaboration with ARM to define
and deliver the first power management application programming
interfaces (API) for ARM® mbed™ platforms. Adding
power management APIs to mbed will bring energy efficiency to
standards-based solutions optimized for ultra-low-power,
battery-operated connected devices. The new APIs will enable the mbed
community of more than 100,000 registered developers to optimize their
mbed-enabled ARM Cortex®-M architecture-based designs for the
utmost energy efficiency and longer battery life.
In addition to enabling developers to manage processor and peripheral
states, the mbed power management APIs are designed with real-world,
low-energy application scenarios in mind. A new feature exposed by the
APIs on Silicon Labs' EFM32® Gecko microcontrollers (MCUs)
automatically determines and enables the optimal sleep mode based on the
MCU peripherals in use, which can dramatically reduce system-level
energy consumption. Low-energy optimization is achieved by enabling I/O
operations to be executed in the background and by allowing those
operations to continue even while the MCU core is in sleep mode or
during other processing tasks.
The automatic selection of the optimal sleep mode, combined with
low-energy, autonomous MCU peripherals, enables developers to
significantly reduce the energy consumption of their IoT applications
with minimal effort. For example, energy profiles of an application
updating a clock display every second on a memory LCD - a common use
case for IoT devices - have shown a current consumption reduction from
1.03 mA to 0.100 mA.
"The new power management APIs for ARM mbed make it possible for
developers to create applications that take advantage of the low-power
features of ARM Cortex-M based microcontrollers," said Zach Shelby, vice
president, IoT business marketing, ARM. "This is an important step
toward enabling full energy-awareness in IoT devices, and it is one of
the key building blocks for mbed OS that is due for public release later
this year."
"As pioneers in low-energy processing solutions for the IoT, Silicon
Labs and ARM have made enormous progress in defining and delivering the
new power management APIs for mbed," said Daniel Cooley, vice president
and general manager of Silicon Labs' MCU and wireless products. "We're
excited to help deliver the industry's first low-power mbed platform,
which will play a key role in accelerating the deployment of countless
battery-powered IoT applications."
Availability
Silicon Labs plans to provide mbed-enabled EFM32
Gecko starter kits in April 2015. Silicon Labs' initial platforms
supporting mbed will include the Wonder Gecko, Leopard Gecko, Giant
Gecko and Zero Gecko starter kits. Developers with existing EFM32 kits
will be able to mbed-enable their hardware through a simple software
update. For more information about Silicon Labs' mbed platforms, please
visit www.silabs.com/mbed.
Silicon Labs
Silicon Labs (NASDAQ: SLAB) is a leading provider of silicon, software
and system solutions for the Internet of Things, Internet
infrastructure, industrial automation, consumer and automotive markets.
We solve the electronics industry's toughest problems, providing
customers with significant advantages in performance, energy savings,
connectivity and design simplicity. Backed by our world-class
engineering teams with unsurpassed software and mixed-signal design
expertise, Silicon Labs empowers developers with the tools and
technologies they need to advance quickly and easily from initial idea
to final product. www.silabs.com
Cautionary Language
This press release may contain forward-looking statements based on
Silicon Labs' current expectations. These forward-looking statements
involve risks and uncertainties. A number of important factors could
cause actual results to differ materially from those in the
forward-looking statements. For a discussion of factors that could
impact Silicon Labs' financial results and cause actual results to
differ materially from those in the forward-looking statements, please
refer to Silicon Labs' filings with the SEC. Silicon Labs disclaims any
intention or obligation to update or revise any forward-looking
statements, whether as a result of new information, future events or
otherwise.
Note to editors: Silicon Labs, Silicon Laboratories, the "S" symbol, the
Silicon Laboratories logo and the Silicon Labs logo are trademarks of
Silicon Laboratories Inc. All other product names noted herein may be
trademarks of their respective holders.
Follow Silicon Labs at http://news.silabs.com/,
at http://blog.silabs.com/,
on Twitter at http://twitter.com/siliconlabs
and on Facebook at http://www.facebook.com/siliconlabs.
Explore Silicon Labs' diverse product portfolio at www.silabs.com/parametric-search.

Silicon Labs
Dale Weisman, +1-512-532-5871
dale.weisman@silabs.com
Source: Silicon Labs
News Provided by Acquire Media