View all news

Silicon Labs Amplifies Innovation for iOS Accessories with Digital Audio Bridge Chip

March 30, 2015

Energy-Friendly CP2614 IC and Evaluation Kit Simplify Accessory Development with Built-in Firmware and Protocol Support

AUSTIN, Texas--(BUSINESS WIRE)-- Silicon Labs (NASDAQ: SLAB), a leading provider of microcontroller, wireless connectivity, analog and sensor solutions for the Internet of Things (IoT), today introduced a digital audio bridge chip and evaluation kit designed to simplify the development of accessories for iOS devices. The new CP2614 interface IC provides a turnkey audio bridge solution for a wide range of Made for iPod/iPhone/iPad (MFi) devices that use the all-digital Lightning connector. Target applications include audio accessories such as guitar and microphone recording dongles, audio docks and headphones. The CP2614 IC also provides built-in support for communication between iOS applications and accessory hardware, enabling a broad array of IoT accessories that operate with a companion iOS app.

Silicon Labs' CP2614 bridge chip and MFI-SL-CP2614-EK evaluation kit provide a cost-effective, comprehensive development platform for iOS accessory developers, enabling fast time to market through fixed-function MFi support. The CP2614 solution requires no firmware development, which helps developers get up and running quickly with their MFi accessory designs. Developers simply select their customization options with an easy-to-use GUI-based configuration tool.

The CP2614 bridge chip carefully manages and minimizes power consumption, achieving ultra-low power in both active and idle modes. The CP2614 IC's exceptional energy efficiency makes it an optimal choice for device-powered accessories. The CP2614 also includes an integrated 5 V low drop-out (LDO) regulator, which reduces bill of materials (BOM) cost and footprint for self-powered accessories. The highly integrated CP2614 device operates without an external crystal or EEPROM, storing all configuration options on chip. The crystal-less architecture and integrated EEPROM further reduce BOM cost as well as printed circuit board (PCB) space, enabling developers to design smaller, more streamlined and cost-effective accessories.

"In designing our pocket-sized iTrack Pocket stereo recording product, we needed a bridge chip solution that could fit the extreme form-factor, low-power and high-quality audio requirements of our device-powered iOS accessory," said Rob Jenkins, director of product engineering at Focusrite, a leading manufacturer of audio recording equipment and the number-one-selling audio interface brand worldwide. "The CP2614 device fit our design needs by offering an ideal combination of small footprint and low current. Our hardware and software audio products make music easy to make, and the CP2614 made the iTrack Pocket easy to make."

The CP2614 audio bridge chip supports 24-bit unidirectional and 16-bit bidirectional digital audio streaming, enabling developers to create high-quality, high-performance "prosumer"-class audio accessories. The CP2614 can establish a communications channel with an iOS application, enabling the app to interact directly with the accessory hardware through general-purpose input/output (GPIO) read/writes and access to the UART for custom data flow. The GPIO can be configured for button input and LED output and accessed remotely from an iOS app or used to control audio playback.

"To succeed in today's competitive iOS accessory market, developers need turnkey solutions - silicon, firmware and evaluation kits - that help them to simplify their designs, reduce power and cost, and speed time to market," said Daniel Cooley, vice president and general manager of Silicon Labs' microcontroller and wireless products. "Our new CP2614 audio bridge chip and evaluation kit enable customers like Focusrite to focus on creating differentiated iOS audio accessory products with innovative features that add value for the end user."

Pricing and Availability

The CP2614 audio bridge IC and MFI-SL-CP2614-EK evaluation kit are in full production and available to MFi licensees today. Available in a 5 mm x 5 mm QFN32 package, the CP2614 IC is priced at $2.51 (USD) in 10,000-unit quantities. The MFI-SL-CP2614-EK is priced at $59 (USD MSRP). MFi licensees can order the evaluation kit through the Apple MFi Procurement Portal. For additional information about the CP2614 audio bridge IC and to order samples, please visit www.silabs.com/interface.

Silicon Labs

Silicon Labs (NASDAQ: SLAB) is a leading provider of silicon, software and system solutions for the Internet of Things, Internet infrastructure, industrial automation, consumer and automotive markets. We solve the electronics industry's toughest problems, providing customers with significant advantages in performance, energy savings, connectivity and design simplicity. Backed by our world-class engineering teams with unsurpassed software and mixed-signal design expertise, Silicon Labs empowers developers with the tools and technologies they need to advance quickly and easily from initial idea to final product. www.silabs.com

Cautionary Language

This press release may contain forward-looking statements based on Silicon Labs' current expectations. These forward-looking statements involve risks and uncertainties. A number of important factors could cause actual results to differ materially from those in the forward-looking statements. For a discussion of factors that could impact Silicon Labs' financial results and cause actual results to differ materially from those in the forward-looking statements, please refer to Silicon Labs' filings with the SEC. Silicon Labs disclaims any intention or obligation to update or revise any forward-looking statements, whether as a result of new information, future events or otherwise.

Note to editors: Silicon Labs, Silicon Laboratories, the "S" symbol, the Silicon Laboratories logo and the Silicon Labs logo are trademarks of Silicon Laboratories Inc. All other product names noted herein may be trademarks of their respective holders.

Follow Silicon Labs at http://news.silabs.com/, at http://blog.silabs.com/, on Twitter at http://twitter.com/siliconlabs and on Facebook at http://www.facebook.com/siliconlabs.

Explore Silicon Labs' diverse product portfolio at www.silabs.com/parametric-search

Silicon Labs
Dale Weisman, +1-512-532-5871
dale.weisman@silabs.com

Source: Silicon Labs

News Provided by Acquire Media

Categories: Press Releases
View all news