Comprehensive Sensorless Brushless DC Motor Control Solution Eases
Application Development, Speeds Time to Market
AUSTIN, Texas--(BUSINESS WIRE)--
Silicon
Labs (NASDAQ: SLAB), a leader in high-performance, analog-intensive,
mixed-signal ICs, today introduced a brushless dc (BLDC) motor control
reference design featuring ready-to-use hardware and software for
sensorless BLDC applications using Silicon Labs' C8051F85x/6x
microcontrollers (MCUs). Silicon Labs' new reference design provides a
comprehensive, system-level solution that accelerates embedded
development for a wide range of motor control applications including
remote control helicopters, motorized toy cars, electronic speed
controllers, PC and electric fans, electric tools such as cutters,
shears, mowers, nail guns and staplers, and small appliances such as
mixers, grinders, toothbrushes and vacuum cleaners.
As embedded system designs continue to increase in complexity and
development schedules grow tighter, reducing development time is a key
consideration in MCU selection for motor control applications. The
C8051F85x/6x MCU-based motor control reference design makes the
developer's job easier by providing cost-effective hardware and
production-quality firmware for quick evaluation and deployment in
cost-sensitive BLDC applications. In addition, the motor control
graphical user interface (GUI) gives developers greater flexibility and
ease-of-use when controlling and understanding BLDC motor operation, and
access to production-ready motor control source code helps to expedite
the design-in time.
The sensorless BLDC motor control reference design uses a C8051F850 MCU
to control a BLDC outrunner motor (typically found in toy helicopters)
mounted on the motor mount board. The powertrain board contains gate
drivers, power MOSFETs, a current sensing resistor as well as resistor
dividers to attenuate motor phase voltages so that they can be measured
by the C8051F85x/6x MCU. The MCU board contains a C8051F85x/6x MCU, as
well as buttons to start/stop and change motor direction and reset the
MCU. The MCU's PWM output drives the gate drivers on the powertrain
board. The MCU board also contains an operational amplifier (op-amp) to
amplify the current sensing voltage so it can be measured by the MCU.
The C8051F85x/6x family is ideally suited for BLDC applications because
of its best-in-class analog performance, small footprint and other
features optimized for motor control designs. The cost-effective,
high-performance 8051-based MCU spins the reference design kit's 6-pole
motor at a maximum speed of 50,000 rpm. The C8051F85x/6x MCU family also
helps developers reduce overall system cost by eliminating the need for
external components such as a crystal oscillator, voltage reference,
level shifters, temperature sensor and other discretes.
Silicon Labs' sensorless BLDC reference design is designed to give
developers a productive, comprehensive "out-of-box" experience,
providing everything needed to get a motor spinning in less than five
minutes. The reference design includes the following hardware and
software tools:
-
C8051F850 MCU control board providing the intelligence to drive the
motor and associated peripherals
-
Powertrain board with gate drivers and power MOSFETs
-
Turnigy 450 Series 3800 kV BLDC outrunner motor attached to a motor
mount board
-
CD with application notes, production-ready motor control firmware
source code and software tools including a motor control GUI
-
Complimentary Keil® PK51 development software with unrestricted
license (an approximate value of $2,500 USD)
-
Power supply and USB cable
"Rapid application development, reduced system cost and fast time to
market mean everything to embedded developers working on cost-sensitive
motor control designs," said Diwakar Vishakhadatta, vice president and
general manager of 8-bit MCU products at Silicon Labs. "We created our
sensorless BLDC motor control reference design to help make the
developer's job easier and more productive and to highlight the
significant benefits in designing BLDC systems based on our popular
C8051F85x/6x MCUs."
Pricing and Availability
Silicon Labs' C8051F850-BLDC-RD motor control reference design is
available today and priced at $164.99 (USD MSRP). Samples and production
quantities of Silicon Labs' C8051F85x/6x MCUs are also available now.
MCU pricing in 10,000-unit quantities begins at $0.40 (USD), and high
volume pricing starts at $0.30.
For additional information about the sensorless BLDC motor control
reference design and to order MCU samples and download complimentary
Keil development tools, please visit www.silabs.com/smallmcu.
Silicon Labs
Silicon Labs is an industry leader in the innovation of
high-performance, analog-intensive, mixed-signal ICs. Developed by a
world-class engineering team with unsurpassed expertise in mixed-signal
design, Silicon Labs' diverse portfolio of patented semiconductor
solutions offers customers significant advantages in performance, size
and power consumption. For more information about Silicon Labs, please
visit www.silabs.com.
Cautionary Language
This press release may contain forward-looking statements based on
Silicon Labs' current expectations. These forward-looking statements
involve risks and uncertainties. A number of important factors could
cause actual results to differ materially from those in the
forward-looking statements. For a discussion of factors that could
impact Silicon Labs' financial results and cause actual results to
differ materially from those in the forward-looking statements, please
refer to Silicon Labs' filings with the SEC. Silicon Labs disclaims any
intention or obligation to update or revise any forward-looking
statements, whether as a result of new information, future events or
otherwise.
Note to editors: Silicon Laboratories, Silicon Labs, the "S" symbol, the
Silicon Laboratories logo and the Silicon Labs logo are trademarks of
Silicon Laboratories Inc. All other product names noted herein may be
trademarks of their respective holders.
Follow Silicon Labs on Twitter at http://twitter.com/silabs
and on Facebook at http://www.facebook.com/siliconlabs.
Explore Silicon Labs' diverse product portfolio at www.silabs.com/parametric-search.

Silicon Labs
Dale Weisman, +1-512-532-5871
dale.weisman@silabs.com
Source: Silicon Labs
News Provided by Acquire Media