AUSTIN, Texas, Aug 17, 2009 (BUSINESS WIRE) -- Silicon Laboratories Inc. (Nasdaq: SLAB), a leader in high-performance,
analog-intensive, mixed-signal ICs, today announced its participation in
the EE Times Virtual Conference on Power Management: Designing for
Efficiency, being held Tuesday, August 18th at www.eetimes.com/power.
Designers can visit Silicon Labs' online booth from their desks and
learn about the company's low power products that are ideal for
addressing design challenges for power delivery, power management and
power efficiency.
Silicon Labs will be showing the industry's highest performance embedded
wireless solution at the virtual exhibition, which combines the
high-performance EZRadioPRO(TM) transceiver family and the C8051F9xx series
of low-power mixed-signal MCUs. High performance coupled with
comprehensive built-in system features, such as packet handling and
antenna diversity, allows the devices to achieve the lowest overall
system cost for frequencies from 240 to 960 MHz. The solution enables
customers to develop embedded wireless solutions that operate from a
single cell battery, reducing cost and size in consumer and industrial
applications such as remote meter reading, home security, remote keyless
entry and building automation.
Live Chat: Low Power Considerations in Embedded Wireless Applications
Silicon Laboratories will be hosting a live online chat: Low Power
Considerations in Embedded Wireless Applications from 4:00 pm - 4:30 pm
EDT on August 18th to discuss how to address conflicting
requirements to add more features while increasing battery life.
Register to participate at www.eetimes.com/power.
Energy Harvesting Webcast
As part of the event, Silicon Laboratories will be participating in a
webcasted panel: Energy Harvesting: From Simple Ideology to Practical
Application, being held online from 1:30 pm - 2:30 pm EDT on August 18th.
The panel will address the practical uses of energy harvesting to
generate power while reducing costs. Register to participate at www.eetimes.com/power.
Silicon Labs' online booth, webcast and chat will be archived until
February 18, 2010.
Silicon Laboratories Inc.
Silicon Laboratories is an industry leader in the innovation of
high-performance, analog-intensive, mixed-signal ICs. Developed by a
world-class engineering team with unsurpassed expertise in mixed-signal
design, Silicon Labs' diverse portfolio of highly-integrated,
easy-to-use products offers customers significant advantages in
performance, size and power consumption. These patented solutions serve
a broad set of markets and applications including consumer,
communications, computing, industrial and automotive.
Headquartered in Austin, TX, Silicon Labs is a global enterprise with
operations, sales and design activities worldwide. The company is
committed to contributing to our customers' success by recruiting the
highest quality talent to create industry-changing innovations. For more
information about Silicon Labs, please visit www.silabs.com.
Cautionary Language
This press release may contain forward-looking statements based on
Silicon Laboratories' current expectations. These forward-looking
statements involve risks and uncertainties. A number of important
factors could cause actual results to differ materially from those in
the forward-looking statements. For a discussion of factors that could
impact Silicon Laboratories' financial results and cause actual results
to differ materially from those in the forward-looking statements,
please refer to Silicon Laboratories' filings with the SEC. Silicon
Laboratories disclaims any intention or obligation to update or revise
any forward-looking statements, whether as a result of new information,
future events or otherwise.
Note to editors: EZRadioPRO, Silicon Laboratories, Silicon Labs, the "S"
symbol and the Silicon Labs logo are trademarks of Silicon Laboratories
Inc. All other product names noted herein may be trademarks of their
respective holders.

SOURCE: Silicon Laboratories Inc.
Silicon Laboratories Inc.
Shannon Pleasant, 512-464-9254
Shannon.pleasant@silabs.com
Copyright Business Wire 2009