AUSTIN, TexasJan. 22, 2009Silicon Laboratories Inc.Wednesday, February 4th,
20097:30 a.m.
Central Timewww.silabs.comBill Bock
A replay will be available after the call at the same website listed
above or by calling 866-516-0673 or +1 203-369-2037 (international).
These replays will be available through February 18th, 2009.
Silicon Laboratories Inc.
Silicon Laboratories is an industry leader in the innovation of
high-performance, analog-intensive, mixed-signal ICs. Developed by a
world-class engineering team with unsurpassed expertise in mixed-signal
design, Silicon Labs' diverse portfolio of highly-integrated,
easy-to-use products offers customers significant advantages in
performance, size and power consumption. These patented solutions serve
a broad set of markets and applications including consumer,
communications, computing, industrial and automotive.
Headquartered in Austin, TX, Silicon Labs is a global enterprise with
operations, sales and design activities worldwide. The company is
committed to contributing to our customers' success by recruiting the
highest quality talent to create industry-changing innovations. For more
information about Silicon Labs, please visit www.silabs.com.
Note to editors: Silicon Laboratories and the Silicon Labs logo are
trademarks of Silicon Laboratories Inc. All other product names noted
herein may be trademarks of their respective holders.
CONTACT: Silicon Laboratories Inc., Austin
Shannon Pleasant, 512-464-9254
shannon.pleasant@silabs.com
Source: Silicon Laboratories Inc.