A replay will be available after the call at the same website
listed above or by calling 800-333-1872 or +1 203-369-3250
(international). These replays will be available through August 13th,
2008.
Silicon Laboratories Inc.
Silicon Laboratories is an industry leader in the innovation of
high-performance, analog-intensive, mixed-signal ICs. Developed by a
world-class engineering team with unsurpassed expertise in
mixed-signal design, Silicon Labs' diverse portfolio of
highly-integrated, easy-to-use products offers customers significant
advantages in performance, size and power consumption. These patented
solutions serve a broad set of markets and applications including
consumer, communications, computing, industrial and automotive.
Headquartered in Austin, TX, Silicon Labs is a global enterprise
with operations, sales and design activities worldwide. The company is
committed to contributing to our customers' success by recruiting the
highest quality talent to create industry-changing innovations. For
more information about Silicon Labs, please visit www.silabs.com.
Note to editors: Silicon Laboratories and the Silicon Labs logo
are trademarks of Silicon Laboratories Inc. All other product names
noted herein may be trademarks of their respective holders.
CONTACT: Silicon Laboratories Inc., Austin
Shannon Pleasant, 512-464-9254
shannon.pleasant@silabs.com
SOURCE: Silicon Laboratories Inc