Easy-to-Use Web-Based Utility Eliminates Guesswork and Enables System Power Budget Assessment in Minutes
The power consumption calculator is especially helpful for power-sensitive and thermally constrained designs in small enclosures such as industrial process control modules or programmable logic controllers. In these and similar designs, the developer must understand the power consumption of every component in the system including the digital isolator.
The calculator is intuitively easy to use. The user simply selects the settings that match the design such as total number of channels, VDD supply voltage and individual channel parameters, and then clicks "Get Results" to obtain detailed power and current data.
Without access to such a tool, the developer would need to extrapolate power specifications from data sheets or conduct extensive calculations and then guess at some of the isolation parameters. The calculator tool eliminates the guesswork. Instead of spending hours studying data sheets, picking parameters and making judgment calls based on systems characteristics to determine the impact on the system power budget, the utility speeds up the entire process to just a few minutes.
"System developers are extraordinarily busy, and we developed the
Isolator Power Consumption Calculator to help simplify the design
process," said
The Isolator Power Consumption Calculator is available free at www.silabs.com/isolator-power-calculator.
It can be used online or downloaded for offline use by developers. The
calculator is one of several web-based utilities developed by
About Silicon Labs Digital Isolators
Silicon Labs' Si84xx and Si86xx digital isolator families use a novel RF isolation architecture fabricated in a standard CMOS to deliver a highly integrated one-to-six-channel isolator that is one-third the size of optocoupler solutions, reducing the cost of the bill of materials by as much as 50 percent. These digital isolators provide a smaller, faster and more reliable isolation solution than optocouplers without the wear-out mechanisms, aging effects or temperature dependencies that plague optocoupler-based designs. Silicon Labs' digital isolators employ an RF coupler to transmit digital information across an isolation barrier, enabling very high-speed operation at low power levels. They also offer best-in-class electromagnetic (EMI) immunity among digital isolation solutions.
Silicon Labs' digital isolators are designed to replace optocouplers in applications requiring robust operation and high levels of insulation protection such as industrial automation and drives, motor control and medical systems. They also provide an ideal isolation solution for systems powered from 220 Vac mains supplies such as isolated ac-dc and dc-dc power supplies, as well as solar panel microinverters, data communications systems and hybrid electric vehicles (HEVs).
Cautionary Language
This press release may contain forward-looking statements based on
Silicon Laboratories' current expectations. These forward-looking
statements involve risks and uncertainties. A number of important
factors could cause actual results to differ materially from those in
the forward-looking statements. For a discussion of factors that could
impact
Note to editors:
Explore Silicon Labs' diverse product portfolio at www.silabs.com/parametric-search.
dale.weisman@silabs.com
Source:
News Provided by Acquire Media