Sony Ericsson Adopts Silicon Laboratories' FM Radio Tuner for the W950 Walkman(R) Phone; Si4701 Offers Superior Performance and Integration

August 7, 2006

®®
The Silicon Laboratories Si4701 incorporates a digital processor for the RDS and the Radio Broadcast Data System (RBDS), which includes all the required RDS/RBDS symbol decoding, block synchronization and error detection and correction functions. This feature enables Sony Ericsson to provide FM broadcast data such as song title, artist, and station name on the W950 Walkman® phone. The Si4701 is pin compatible to the non-RDS part, the Si4700.

"Consumers are demanding handsets with music functionality for both feature-rich phones and entry-level handsets," said Tyson Tuttle, vice president of Silicon Laboratories. "The performance, integration and ease-of-use of our FM tuner products allow manufacturers like Sony Ericsson to quickly implement world-class FM stereo as a standard feature on any handset or portable media device."

The Si4701 reduces cost while enabling superior sound quality and adjustability in critical FM receiver specifications. Using patented technology including a field-proven, low IF digital architecture and embedded processor technology, Silicon Laboratories' FM tuners offer industry-leading performance in all FM receiver specifications and excel in real-world environments such as large cities where high immunity to blockers is critical for good reception. The devices provide software programmability for the seek, soft mute and stereo blend parameters, all of which are fundamental to superior performance in highly variable FM broadcast environments.

Silicon Laboratories Inc.

Silicon Laboratories Inc. is a leading designer of high-performance, analog-intensive, mixed-signal integrated circuits (ICs) for a broad range of applications. Silicon Laboratories' diverse portfolio of highly integrated, patented solutions is developed by a world-class engineering team with decades of cumulative expertise in cutting-edge mixed-signal design. The company has design, engineering, marketing, sales and applications offices throughout North America, Europe and Asia. For more information about Silicon Laboratories please visit www.silabs.com.

Cautionary Language

This press release may contain forward-looking statements based on Silicon Laboratories' current expectations. These forward-looking statements involve risks and uncertainties. A number of important factors could cause actual results to differ materially from those in the forward-looking statements. For a discussion of factors that could impact Silicon Laboratories' financial results and cause actual results to differ materially from those in the forward-looking statements, please refer to Silicon Laboratories' filings with the SEC. Silicon Laboratories disclaims any intention or obligation to update or revise any forward-looking statements, whether as a result of new information, future events or otherwise.

Note to editors: Silicon Laboratories and the Silicon Laboratories logo are trademarks of Silicon Laboratories Inc. All other product names noted herein may be trademarks of their respective holders. In the term "mm2" above, the "2" is a superscript numeral. It was changed for transmission purposes only.

CONTACT: Silicon Laboratories Inc., Austin
Kirstan Ryan, 512-532-5349
kirstan.ryan@silabs.com

SOURCE: Silicon Laboratories Inc.