Press Release

<< Back
Sep 19, 2018
Silicon Labs' Wireless Xpress Modules Deliver Bluetooth and Wi-Fi Connectivity with Zero Programming
-- Prototype IoT Applications in One Day with Drop-and-Connect Simplicity --

AUSTIN, Texas, Sept. 19, 2018 /PRNewswire/ -- Silicon Labs (NASDAQ: SLAB) offers a new Wireless Xpress solution to help developers get IoT applications connected and running in a day, with no software development necessary. Silicon Labs' Wireless Xpress provides a configuration-based development experience with everything developers need including certified Bluetooth® 5 Low Energy (LE) and Wi-Fi® modules, integrated protocol stacks and easy-to-use tools.

Silicon Labs' Wireless Xpress helps developers get IoT applications connected and running in a day, with no software development necessary.

"By using Bluetooth and Wi-Fi Wireless Xpress, developers can move from product concept to prototyping in a matter of hours instead of weeks," said Matt Johnson, Senior Vice President and General Manager of IoT products at Silicon Labs. "Wireless Xpress greatly reduces the design learning curve without compromising sophisticated Bluetooth or Wi-Fi functionality. Developers will spend less time learning how to add wireless connectivity to their IoT devices and more time designing innovative, distinctive products and getting them to market ahead of the competition."

With on-board wireless stacks controlled through a high-level Xpress Command API for setup and control, Wireless Xpress devices require only modest resources from a host processor, enabling developers to add wireless connectivity to any microcontroller (MCU).

Bluetooth and Wi-Fi IoT products based on Wireless Xpress can be remotely managed and updated over the air (OTA) using native device management features. With Silicon Labs' Zentri device management service (DMS), end users can easily install and update firmware, view real-time device health metrics and adjust product settings through mobile apps.

To ease the complexity of adding Bluetooth or Wi-Fi connectivity to mobile applications, Wireless Xpress includes a mobile app SDK for Android and iOS. The mobile app framework comprises examples and libraries and offers simple communications and OTA APIs to accelerate app development and simplify wireless design for mobile platforms.

Wireless Xpress takes advantage of Silicon Labs' Gecko OS, an intuitive, simple-to-use IoT operating system that accelerates the development of market-ready connected products. Silicon Labs plans to offer additional Gecko OS-based products and solutions in the future.

Bluetooth LE Xpress Solution Highlights

  • Bluetooth 5 BGX13 module requiring no firmware development
  • Zero-overhead serial-to-Bluetooth cable replacement solution
  • Smartphone app for Bluetooth LE command, control and sensing
  • Secure connections with encrypted communication, bonding and passkey pairing
  • Ideal solution for smart home products requiring Bluetooth control with a mobile app and adding a point-to-point wireless interface to industrial applications

Wi-Fi Xpress Solution Highlights

  • Streamlines cloud connectivity with low-power Wi-Fi modules and software
  • Supports cloud vendors including Amazon AWS and Microsoft Azure
  • Integrated web app enabling browser-based user interfaces
  • Ideal for applications such as home appliances, wireless sensing, thermostats, IP cameras and health monitoring requiring direct Internet access and remote provisioning and updates

Pricing and Availability
Silicon Labs' Bluetooth LE BGX13P and BGX13S modules are available today in a choice of pre-certified PCB and SiP modules, respectively, with integrated antenna options. The Wi-Fi AMW007 and AMW037 PCB modules are also available today. Module pricing begins at $4.09 USD in 10,000-unit quantities. Wireless Xpress evaluation kits are available now and priced at $40 (MSRP USD). Developers can download the Wireless Xpress SDK with code examples through Simplicity Studio. Wireless Xpress mobile apps for Android and iOS are available at https://github.com/siliconlabs/wireless-xpress. To learn more about Wireless Xpress solutions, visit www.silabs.com/wireless-xpress.

Silicon Labs
Silicon Labs (NASDAQ: SLAB) is a leading provider of silicon, software and solutions for a smarter, more connected world. Our award-winning technologies are shaping the future of the Internet of Things, Internet infrastructure, industrial automation, consumer and automotive markets. Our world-class engineering team creates products focused on performance, energy savings, connectivity and simplicity. www.silabs.com

Connect with Silicon Labs
Silicon Labs PR Contact: Dale Weisman +1-512-532-5871, dale.weisman@silabs.com

Follow Silicon Labs at http://news.silabs.com/, at http://blog.silabs.com/, on Twitter at http://twitter.com/siliconlabs, on LinkedIn at http://www.linkedin.com/company/siliconlabs and on Facebook at http://www.facebook.com/siliconlabs.

Cautionary Language
This press release may contain forward-looking statements based on Silicon Labs' current expectations. These forward-looking statements involve risks and uncertainties. A number of important factors could cause actual results to differ materially from those in the forward-looking statements. For a discussion of factors that could impact Silicon Labs' financial results and cause actual results to differ materially from those in the forward-looking statements, please refer to Silicon Labs' filings with the SEC. Silicon Labs disclaims any intention or obligation to update or revise any forward-looking statements, whether as a result of new information, future events or otherwise.

Note to editors: Silicon Labs, Silicon Laboratories, the "S" symbol, the Silicon Laboratories logo and the Silicon Labs logo are trademarks of Silicon Laboratories Inc. All other product names noted herein may be trademarks of their respective holders.

 

Cision View original content to download multimedia:http://www.prnewswire.com/news-releases/silicon-labs-wireless-xpress-modules-deliver-bluetooth-and-wi-fi-connectivity-with-zero-programming-300712568.html

SOURCE Silicon Labs