New Wireless Software from Silicon Labs Enables Bluetooth Communications with Sub-GHz IoT Devices
AUSTIN, Texas, June 13, 2018 /PRNewswire/ -- Silicon Labs (NASDAQ: SLAB) has released new software options for its Wireless Gecko portfolio, enabling simultaneous sub-GHz and 2.4 GHz Bluetooth® Low Energy (LE) connectivity on a single chip. This Silicon Labs solution enables commercial and industrial IoT applications to combine long-range sub-GHz communications with Bluetooth connectivity, simplifying device setup, data gathering and maintenance. By avoiding the complexity of two-chip wireless architectures, developers can speed time-to-market and reduce bill-of-materials (BOM) cost and size by up to 40 percent.
Silicon Labs' new Wireless Gecko hardware and software solution enables users to set up, control and monitor sub-GHz IoT devices directly over Bluetooth with mobile apps. By adding Bluetooth LE connectivity to wireless networks in the sub-GHz band, developers can deliver new capabilities such as faster over-the-air (OTA) updates and deploy scalable, location-based service infrastructure with Bluetooth beacons.
Proprietary sub-GHz protocols are commonly used in low-data-rate systems, from simple point-to-point connections to large mesh networks and low-power wide area networks (LPWAN), where extended range, robust radio links and energy efficiency are top priorities. Sub-GHz connectivity is a good fit for long-range wireless sensor networks, smart metering, home and building automation, and commercial lighting. Silicon Labs' Wireless Gecko solution makes it easy to add Bluetooth LE connectivity to these sub-GHz applications.
"Sub-GHz wireless protocols are widespread in smart energy, industrial and commercial applications," said Lee Ratliff, Senior Principal Analyst, Connectivity and IoT, at IHS Markit. "Ubiquitous support of Bluetooth in mobile devices has created demand for multiband, multiprotocol wireless solutions that can bridge the gap between Bluetooth LE and sub-GHz proprietary protocols, enabling legacy applications to leverage the power of the mobile device ecosystem."
"Silicon Labs' new software makes it easier to set up and manage a wide range of sub-GHz wireless devices in the field through easy-to-use mobile apps and Bluetooth connectivity," said Dennis Natale, Vice President and General Manager of IoT products at Silicon Labs. "Our Wireless Gecko portfolio provides a single-chip solution that reduces design costs, simplifies hardware and software development, and accelerates time to market."
Silicon Labs is a leading provider of silicon, software and solutions for a smarter, more connected world. The company offers more than 20 years of experience delivering integrated RF solutions and has shipped more than 750 million wireless devices for IoT end nodes.
Pricing and Availability
Silicon Labs' new multiprotocol software is available now to customers using Silicon Labs' EFR32MG and EFR32BG Wireless Gecko SoCs. Silicon Labs provides comprehensive software tools to simplify sub-GHz and Bluetooth development, including a connected lighting demonstration and a sample mobile application. Contact a local Silicon Labs sales representative or authorized distributor for EFR32 Wireless Gecko SoC pricing. To get started and learn more, visit www.silabs.com/dynamic-multiprotocol.
Silicon Labs
Silicon Labs (NASDAQ: SLAB) is a leading provider of silicon, software and solutions for a smarter, more connected world. Our award-winning technologies are shaping the future of the Internet of Things, Internet infrastructure, industrial automation, consumer and automotive markets. Our world-class engineering team creates products focused on performance, energy savings, connectivity and simplicity. www.silabs.com
Connect with Silicon Labs
Silicon Labs PR Contact: Dale Weisman +1-512-532-5871, dale.weisman@silabs.com
Follow Silicon Labs at http://news.silabs.com/, at http://blog.silabs.com/, on Twitter at http://twitter.com/siliconlabs, on LinkedIn at http://www.linkedin.com/company/siliconlabs and on Facebook at http://www.facebook.com/siliconlabs.
Cautionary Language
This press release may contain forward-looking statements based on Silicon Labs' current expectations. These forward-looking statements involve risks and uncertainties. A number of important factors could cause actual results to differ materially from those in the forward-looking statements. For a discussion of factors that could impact Silicon Labs' financial results and cause actual results to differ materially from those in the forward-looking statements, please refer to Silicon Labs' filings with the SEC. Silicon Labs disclaims any intention or obligation to update or revise any forward-looking statements, whether as a result of new information, future events or otherwise.
Note to editors: Silicon Labs, Silicon Laboratories, the "S" symbol, the Silicon Laboratories logo and the Silicon Labs logo are trademarks of Silicon Laboratories Inc. All other product names noted herein may be trademarks of their respective holders.
View original content with multimedia:http://www.prnewswire.com/news-releases/new-wireless-software-from-silicon-labs-enables-bluetooth-communications-with-sub-ghz-iot-devices-300665090.html
SOURCE Silicon Labs
News Provided by Acquire Media